Part Number: PROCESSOR-SDK-AM62A
Tool/software:
This issue was reported with SDK 10, and still reproduces with SDK 11.1:
U-Boot SPL 2025.01-00547-g3bcfad6cee95 (Jul 23 2025 - 16:49:22 +0000) SYSFW ABI: 4.0 (firmware rev 0x000b '11.1.5--v11.01.05 (Fancy Rat)') DM ABI: 3.0 (firmware ver 0x000b 'MSDK.11.01.00.16-dirty--v11.01.02' patch_ver:) Trying to boot from MMC2 Error reading cluster spl_load_image_fat: error reading image u-boot.img, err - -22 SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ###
The image boots correctly with a 32 GB SanDisk Ultra microSD card, but does not boot with a 128 GB card of the same make and model (which works with SDK 9.2).
It is a known SW issue, discussed previously with TI team.