This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

can we get AM3715 test examples for camera module?

Other Parts Discussed in Thread: AM3715, DM3730

Hi,

              We use AM3715 cpu to develop new product now , the hardware platform has completed,

but we find it is diffcult to set so many registers about camera module  and dispaly controller . do you

have test examples? how can we get it?

Thanks and best regards

 ---Jerry

 

  • Hi Jerry,

                Mistral AM/DM3730 EVM Kit has a Parallel Camera interface proven with MT9T111 sensor -  Leopard Imaging Camera. If your intention is to understand the register settings and the flow work, you can download the source code from of the diagnostic routine @ U-Boot level named ITBOK downloaded from http://www.mistralsolutions.com/pes-support/support-downloads/amdm37x-evm-documentation-a-software.html

    You might also find these wiki links helpful:

    http://processors.wiki.ti.com/index.php/Camera_Users_Guide

    http://processors.wiki.ti.com/index.php/ITBOK

     

    Regards,

    N.S.SriHarsha

     

  • Hi  N.S.SriHarsha,


               Thanks for your answer, it is very useful for me to understand camera module of AM3715 .

    Regards

    jerry


  • Hi Jerry,

    Alternatively the same mistral kit also has support for the AM3715 processor for other couple of camera modules from e-con Systems.  Here is one of them http://www.e-consystems.com/5mp_hdcamera_AM-DM37x.asp.

    There are also other camera modules available for the same processor. You can get more details from http://www.e-consystems.com/cameramodule.asp. Support is available for Android, Linux and WinCE 6.0.  There is an option for both S mount(Custom lens ) and normal plastic lens options.

    Thanks,

    Lakshmi