Hello Champs,
I would like to know if a USB hub can be supported on Android 2.2/2.3 on Beagle board C4/C5.
if yes, can you please share some guidelines?
We actually needed an SBC with 512 MB Nand which can support NFS. So as per your wiki, we will use USB Host port to connect to the Ethernet. However, can this connection be done via an USB Hub, as we need more USB ports on the OMAP3530 based board?
Best Regards
Feroz