This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3517-EVM Boot issue

Other Parts Discussed in Thread: AM3517

After getting my Ubuntu Linux virtual machine running on VirtualBox, I am able to get the serial message via minicom.

The boot process takes minutes to occur from switch power on to on-screen graphics.

The messages indicate many errors during boot.

I believe they indicate a bad NAND flash.

Is there a corrrection I can make or will I need to replace my eval board?

 

Early boot messaging:

 

Starting X-loader on MMC                                                       
Reading boot sector                                                            
                                                                               
218976 Bytes Read from MMC                                                     
Starting OS Bootloader from MMC...                                             
Starting OS Bootloader...                                                      
                                                                               
                                                                               
U-Boot 2009.11 (Jan 22 2011 - 01:45:10)                                        
                                                                               
OMAP34xx/35xx-GP ES1.0, CPU-OPP2 L3-165MHz                                     
AM3517EVM Board + LPDDR/NAND                                                   
I2C:   ready                                                                   
DRAM:  256 MB                                                                  
NAND:  512 MiB                                                                 
err_loc=2509                                                                   
err_loc=-1144                                                                  
err_loc=-1311                                                                  
err_loc=-2375                                                                  
err_loc=3924                                                                   
err_loc=3686                                                                   
err_loc=959                                                                    
err_loc=-3521                                                                  
err_loc=3535                                                                   
err_loc=2218                                                                   
err_loc=-1854                                                                  
err_loc=-1959                                                                  
err_loc=1141                                                                   
err_loc=559                                                                    
err_loc=-860                                                                   
err_loc=-2114                                                                  
*** Warning - bad CRC or NAND, using default environment