This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515 eZdsp - No data from AIC?

I'm trying to run the example code from 

http://code.google.com/p/c5505-ezdsp/ 

specifically the audio filter demo for the c5515

The code compiles succesfully and runs, but I hear no audio on the output on the board when audio is sent in from an mp3 player. When I use the memory view to inspect the contents of the incoming data buffers, they seem to only contain zeros.

I also added a dma_count variable which is incremented every time there is a DMA interrupt, which appears to be getting interrupted which should show that the I2S config is correct on both ends. I can modify the code to reverse the master/slave configuration and I get the same behaviour.

I think this may be a hardware fault also. The first few times I tried running this demo, I had the same issue. However, it did work and successfully filter audio a few times before going back to the above behaviour again. It doesn't seem to be a software issue as there were minimal changes, and the sample code should work anyway without change, right?

In a couple of weeks I will have some limited access to an oscilloscope so I should be able to give detail about what is appearing on the busses. In the meantime any advice would be appreciated.