Tool/software:
Hii
I'm working on a TI J721E EVM, and during boot, I'm encountering an issue where the psplash-start service fails to start due to a missing /dev/fb0. Below is the relevant error output:
root@j721e-evm:~# systemctl status psplash-start.service
x psplash-start.service - Start psplash boot splash screen
Loaded: loaded (/usr/lib/systemd/system/psplash-start.service; enabled; preset: enabled)
Active: failed (Result: exit-code) since Tue 2024-02-27 17:26:12 UTC; 1min 29s ago
Process: 480 ExecStart=/usr/bin/psplash (code=exited, status=255/EXCEPTION)
Main PID: 480 (code=exited, status=255/EXCEPTION)
CPU: 3ms
Feb 27 17:26:12 j721e-evm systemd[1]: Starting Start psplash boot splash screen...
Feb 27 17:26:12 j721e-evm psplash[480]: Error opening /dev/fb0
Feb 27 17:26:12 j721e-evm systemd[1]: psplash-start.service: Main process exited, code=exited, status=255/EXCEPTION
Feb 27 17:26:12 j721e-evm systemd[1]: psplash-start.service: Failed with result 'exit-code'.
Feb 27 17:26:12 j721e-evm systemd[1]: Failed to start Start psplash boot splash screen.
root@j721e-evm:~# ls /dev/f*
/dev/full /dev/fuse
/dev/fd:
0 1 2 3
Observed Errors during Boot:
So,
-
/dev/fb0is missing during boot. -
psplashfails withError opening /dev/fb0. -
This leads to the failure of
psplash-start.service. -
I'm running this on a J721E EVM board using prebuilt image.
- I want to know root cause for this error
- I want the proper solution for this error.
- Also will this effect the display part , as i m not getting display also .
Thanks
Regards,
Komal