This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VGA monitor detecton on DM8168

Hello :

Some chips has the loading sensor circuit to detect that the montor is connected or disconnected through the 75 ohm double termination on RGB.

Can DM8168 implement this function ?