Part Number: TDA4VH-Q1
Tool/software:
I am implementing a DMA priming setup that operates on a wait-based polling mechanism rather than event-driven mechanism. Given that I have multiple queue operations, I need to understand the optimal approach for dequeue operations. Specifically:
- Should each queue call be paired with a corresponding dequeue operation, or can the dequeue process be optimized?
- Ex: If I have 4 sequential Udma_ringQueueRaw() calls, should there be 4 corresponding Udma_ringDequeueRaw() calls, or can a single dequeue call handle multiple queued operations efficiently?
- Are there more efficient polling strategies that could improve performance while maintaining the wait-based architecture?
I would appreciate insights on best practices for optimizing polling-based DMA queue management.