This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5748: Enabling UART6 at U-boot to Configure GPS chip

Part Number: AM5748

Tool/software:

Hi,

We are  trying to Enable UART6 at u-boot using mw.b md.b commands,  But Clock is not enabling

below is the Address we used to enable clock

mw.b 0x4A005580 0x2                // writing 0x2 to CM_IPU_UART6_CLKCTRL register

=> md.b 0x4A005580 4               // reading to check weather module is enabled or not
4a005580: 02 00 03 00  

We tried to add uart6 node in dts also but didn't help

below is the pinmux we did
        {GPMC_A4,(M8 |  PIN_INPUT )},                                   /* uart6_rxd */
        {GPMC_A5,(M8 |  PIN_OUTPUT )},                                  /* uart6_txd */
        {GPMC_A6,(M8 |  PIN_OUTPUT )},                                  /* uart6_ctsn */
        {GPMC_A7,(M8 |  PIN_OUTPUT )},                                  /* uart6_rtsn */

used u-boot version :u-boot-2018.01

If we do clock enable for  uart5  that is working,  Can you Explain why particularly UART6 Module is not enabling and provide detailed procedure to enable UART at Uboot stage. 

Regards
Yashwanth