Hello TI,
I am running SWOSD demo given in DVRRDK_01.08.00.15 release, it works well when i run it as default code (in which Bool osdFormat was set to 1) but as i want to perform SWOSD on YUV420SP data, as mentioned in code i have to set osdFormat to 0. I did the same as mentioned but i didn't get TI logo as an overlay on display or neither i get statistics that shows DSP processing at the end when i stop the demo in this case.
Can anyone help me out to resolve this issue ?
Do i missed something to enabled other than this (as i mentioned osdFormat =0) ?
Waiting for replay from TI.
Thanks & Regards,
HiteshV