Hi,
I'm using SYS/BIOS as OS for my app on an EVM6678L board with CCS 5.1.3 . When I open my .cfg file, the semaphore module is not present in the outline view which is expected because I haven't "use" the module. I open the BIOS module's property page and then the "system overview" page.The "system overview" shows all the modules that my app uses.What's strange is that the Semaphore module is checked with a green tick which means the module is used. I click on Semaphore module to open its property page and find that the"add Semaphore to ..." box is checked. I try to uncheck the box but it won't work. Since the semaphore module is used but not visible in outline view, I can't statically declare a semaphore. I can create semaphore at runtime as a workaround but I just want to know the cause of the problem.
Thanks,
Roy