Other Parts Discussed in Thread: TPS65987DDK, TPS65981
Tool/software:
Hi,
I'm trying to load TPS65987DDK over i2c with Linux driver ti,tps6598x.
I'm getting a response:
kernel: tps6598x 3-0020: Update completion failed (-16)
Basically, I saved a "Full Flash Image" using the TPS65981 Application Customization software.
Is this binary the correct binary to use? It calls:
tps6598x_exec_cmd(tps, "PTCc", 0, NULL, TPS_PTCC_OUT_BYTES, out);
And this has the wrong bits set:
Also, after I see the firmware update fails, I see that it's trying to activate the usb tty on this device:
cdc_acm 1-1.4:1.0: skipping garbage
cdc_acm 1-1.4:1.1: ttyACM0: USB ACM device
Any tips for how to resolve this issue?