This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: PCIE_DAT2 address

Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH, AM62P, AM67

Tool/software:

Hi,

In the TDA4VH TRM, in paragraph concerning PCIe CBA Infrastructure, it is spoken about PCIE_DAT2 region "used to route all requests with casel not equal to zero to the PCIe controller slave port".

Which is the address of this region, as it is not listed neither in the TRM memory map, nor in the Excel file.

Thank in advance,

JPH

  • Hi JPH,

    I am not finding info either. Let me check internally on this.

    Regards,

    Takuma

  • Hi Takuma,

    Did you get information on this subject ?

    Thanks,

    JPH

  • Hi JPH, 

    No info for PCIE_DAT2. Looked through our older revision TRMs and TRM of older devices that reuse the same IPs. For everything I looked through, PCIE_DAT2 is only mentioned in the single paragraph that you have found.

    Software driver only defines DAT0 and DAT1 spaces as well.

    Regards,

    Takuma

  • Hi JPH,

    So, I got some info from the broader team. PCIE_DAT2 is mainly for address translation bypass, so there is no specific address for this region. It is the 2^48 Byte window in the 48-bit local address space, where translation between device address and PCIe address does not occur. This is the reason why there is no memory region similar to DAT0 and DAT1 space listed in excel sheet.

    Regards,

    Takuma

  • Hi Takuma,

    Thanks for this information.

    I understand that when the DMA’s CASEL (or ASEL?) field is set,  I can use any 48-bit address to access the slave PCIe controller. Did I get that right?

    If so, that would mean that if my PCIe fabric uses 64-bit addressing, I would only be able to address endpoints whose 16 most significant address bits are 0. Is that correct?

    Thanks,

    JPH

  • Hi JPH,

    Non-zero ASEL value will result in outbound ATU bypass. This is useful when the PCIe Controller is acting as an Endpoint and needs to read from or write to the remote Root-Complex's memory. Without outbound ATU bypass, the outbound ATU has to be setup to translate local (EP) address read/write transactions to PCIe Bus address transactions targeting the remote Root-Complex's memory. With ATU bypass, the local address can be identical to the remote Root-Complex's memory itself except for the ASEL bit which will be removed before the address is sent out over the PCIe link without translation - Bits 0 to 47 of the local address will be used as the read/write transaction address on the PCIe link as well.

    PCIen_DAT0 => 128 MB window in the 32-bit Local Address Space => Translated by ATU to generate an address targeting a buffer in the PCIe Root-Complex's memory
    PCIen_DAT1 => 4 GB window in the 64-bit Local Address Space => Translated by ATU to generate an address targeting a buffer in the PCIe Root-Complex's memory
    PCIen_DAT2=> 2^48 Byte window in the 48-bit Local Address Space => Untranslated address identical to the buffer address in PCIe Root-Complex's memory

    Regards,

    Takuma

  • Hi Takuma,

    Thanks for the clarification.

    I just need extra information about the ASEL bit: reading your sentence, it seems that ASEL bit is in the same word as the  destination address, and that it will be removed by the hardware.

    Does the user has to set this bit in the address word ? At which position? I didn't read such information anywhere.

    Thank,

    JPH

  • Hi JPH,

    Bits 48 to 51 of every address correspond to ASEL. SoC Memory Map documented in the T.R.M. corresponds to ASEL 0. ASEL 1 is PCIE0's DAT2, ASEL 2 is PCIE1's DAT2 and so on. 

    PCIe related driver/dts currently just uses 0 as the ASEL, similar to most other interfaces. The main example I know of in Linux SDK that does not use a non-zero ASEL is the CPSW dts for J722S/AM62P where it uses the ASEL value of 15 in the dmas property to route data to the ACP for cache coherence: https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/tree/arch/arm64/boot/dts/ti/k3-am62p-j722s-common-main.dtsi?h=ti-linux-6.12.y#n711

    Regards,

    Takuma 

  • Hi Takuma,

    Thanks again, your answer is very interesting, I did'nt get this information.

    Is there a document where the ASEL subject is detailled ? 

    If you have an example of non zero ASEL on C7x, I am interested.

    Thanks,

    JPH

  • Hi JPH,

    My understanding for ASEL is that it is only relevant for cache coherency on the A53 cores for the AM67, AM64, AM62P, and maybe other Sitara family devices that do not have a MSMC memory in front of the A-core clusters so that data can be routed to ACP for cache coherence, and also relevant for PCIe for address translation bypass. Example I shared in my previous response is for J722S (AM67) and AM62P to show how ASEL can be set in devicetree. TDA4VH has a MSMC so it does not need to use ACP from ARM A core.

    As such, we do not have any examples for C7x that uses non-zero ASEL.

    Regards,

    Takuma