Other Parts Discussed in Thread: AM1808
Dear all,
With reference to AM335x Technical Reference Manual (Rev. C), section "26.1.5.2.1 SYSBOOT Configuration Pins", could you please clarify note 5 related to USB0 boot device?
"5. Boot mode is not a permanent booting device. All other boot modes are and will be included in subsequent booting sequences after each watchdog timeout."
Which is the meaning of "permanent booting device"?
I'm interested in using USB interface for programming empty flash memory of the device at the first time. In my understanding, due to the limit of 110 KB available in internal RAM, it will be necessary to download a Secondary-Boot-Loader to initialize external RAM and other peripheral. Then the SBL will download u-boot etc and write them to flash. Something similar to UART boot mode, but faster (in my expectation). Is it correct?
Thanks in advance.
Best regards,
Max