Other Parts Discussed in Thread: FLASHTOOL
Hi all,
I have a interesting boot problem. I am using Am/Dm 3730 Mistral OMAP3 EVM. I set the sw4 swithces to boot from SD Card, but EVM not booting. Neither X-Loader nor U-Boot booting. Than I changed SW4 switches ro boot from UART3 via FlashTool 1.6 but again not booted. EVM did not send its ASIC ID. I was working for a 3 months on this EVM everything was OK. But now i couldnt boot the EVM. Only one way I can boot the EVM. When i connect whith an emulator from JTAG and init the EVM with the gel files and run from emulator it is booting. After turn off and turn on the EVM not boot without initialization of emulator.
How can i solve this problem friends?
I need to boot without emulator, like before.
Regards,
Ahmet