My team (DSP newbies) are trying to implement a project to capture 8 slots of a TDM stream using the McBSP, EDMA3 and DDR2 in a ping pong buffer fashion. Unfortunately, with so many combinations of BIOS, PSPs, CSLs, BSLs, etc, we have been unable to get a single example project using any of the above modules to build correctly. My team seems to have tried every combination of CCS version, BIOS version and package versions. At this point, I settle for starting from scratch and getting just a few segments building correctly.
So, my real question is:
If I was starting from scratch using an TMS320C6424 EVM from spectrum digital with the end goal of building/using example code for the McBSP, EDMA3, and DDR2; What CCS version should I install, and what supporting packages should I install after that, and then what example should I start with, and finally are there any configuring changes I need to make to have it all work.
BTW: This is being built/installed on a Windows 7 64bit machine if that makes any difference.
Thanks,
Lorin