This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62L: eMMC boot failure

Part Number: AM62L

Tool/software:

Hii, 

I am using AM62L microprocessor. I flashed image on eMMC. My bootmode switch configurations are: 

Pins  Boot Mode Options pins  Details of pins  Primary eMMC/Backup SD card 
1 B0 PLL Reference Clock Selection 1
2 B1 1
3 B2 0
4 B3 Primary Boot Mode Selection 0
5 B4 0
6 B5 0
7 B6 1
8 B7 0
9 B8 0
10 B9 0
11 B10 Backup Mode Selection 1
12 B11 0
13 B12 1
14 B13 0
15 B14 Full/Half Pin Selection  0
16 B15 0

But I found below boot failure logs: 


switch to partitions #0, OK
mmc0(part 0) is current device
SD/MMC found on device 0
610 bytes read in 0 ms
Loaded env from uEnv.txt
Importing environment from mmc0 ...
MMC: no card present
** Bad device specification mmc 1 **
MMC: no card present
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
MMC: no card present
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:2
Can't set block device
Working FDT set to 88000000
Bad Linux ARM64 Image magic!
Scanning for bootflows in all bootdevs
Seq  Method       State   Uclass    Part  Name                      Filename
---  -----------  ------  --------  ----  ------------------------  ----------------
Scanning bootdev 'mmc@fa10000.bootdev':
  0  efi          ready   mmc          1  mmc@fa10000.bootdev.part_ /EFI/BOOT/BOOTAA64.EFI
** Booting bootflow 'mmc@fa10000.bootdev.part_1' with efi
MMC: no card present
Cannot persist EFI variables without system partition
Booting /\EFI\BOOT\BOOTAA64.EFI
error: no such device: ((hd0,msdos1)/EFI/BOOT)/EFI/BOOT/grub.cfg.
error: serial port `com0' isn't found.