Hi,all
I have got a problem those days. I am using DM6437,but not the EVM board. I can access the DM6437 address through PCI, and I can download program to L2,The program ( led blink test program )runs well in L2,but I can't write or read DDR2. when I wrote 0x55aa55aa to the 0x80000000, when read I just got 0xfffffff or 0x0000000.
My DDR2 is NT5TU64M16DG,
DDR_SDBCR = 0x00138833;
DDR_SDTIMR = 0
|(19<<25) // tRFC = ( 125 ns / 6.17 ns ) - 1
| ( 1 << 22 ) // tRP = ( 15 ns / 6.17 ns ) - 1
| ( 1 << 19 ) // tRCD = ( 15 ns / 6.17 ns ) - 1
| ( 1 << 16 ) // tWR = ( 15 ns / 6.17 ns ) - 1
| ( 6 << 11 ) // tRAS = ( 45 ns / 6.17 ns ) - 1
| ( 8 << 6 ) // tRC = ( 60 ns / 6.17 ns ) - 1
| ( 1 << 3 ) // tRRD = ( (4*10ns + 2*6.17ns) / 4*6.17ns ) - 1
| ( 0 << 0 ); // tWTR = ( 7.5 ns / 6.17 ns ) - 1
DDR_SDTIMR2 = 0
| ( 12 << 16 ) // tXSNR= ( 85 ns / 6.17 ns ) - 1
| ( 199 << 8 ) // tXSRD= ( 200 - 1 ) cycles
| ( 0 << 5 ) // tRTP = ( 7.5 ns / 6.17 ns ) - 1
| ( 2 << 0 ); // tCKE = ( 3 - 1 ) cycles
Is there any one who can give me some suggestion ?
I am expecting your reply .
thank you very much!