Other Parts Discussed in Thread: OMAP-L138, DA8XX, OMAP-L137
Hello!
We have developed our customer board based on OMAP-L138. In the first step our device electrical schema is based on SOM and BaseBoard from LogicPD. And now I try to start our device. I have writen UBL and u-boot to SPI flash. My current target is starting of Linux. And I have met a problem. Due to unknown reason Linux can't mount sd card. This is last string of booting log:
Waiting for root device /dev/mmcblk0p2
I have tried to start Linux from different places like SPI flash and SD card FAT partition. But the result is identical. I think that SD card is working normal because u-boot can detect it. But I don't understand why Linux can't do that. I have tried my Linux image in BaseBoard with SOM and it detect SD.
Also I have tried different SD cards. I have tried to load fs from first partiton of SD.
Can anybody give me advices how to solve my problem?
I use PSP SDK 03.20.00.14.
There is my booting log. Also I added pinmux output.
OMAP-L138 initialization passed!
Booting TI User Boot Loader
UBL Version: 1.65
UBL Flashtype: SPI
Starting SPI Memory Copy...
Valid magicnum, 0x55424CBB, found at offset 0x00010000.
DONE
Jumping to entry point at 0xC1080000.
U-Boot 2009.11 (Nov 09 2010 - 18:48:43)
I2C: ready
DRAM: 64 MB
MMC: davinci: 0
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 150000000 Hz
Invalid MAC address read.
Net: Ethernet PHY: GENERIC @ 0x00
Hit any key to stop autoboot: 3 2 1 0
reading boot.scr
** Unable to read "boot.scr" from mmc 0:1 **
reading uImage
2058304 bytes read
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.33-rc4
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2058240 Bytes = 2 MB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.33-rc4 (root@lesha-desktop) (gcc version 4.3.3 (Sourcery G++ L
ite 2009q1-203) ) #15 PREEMPT Tue Dec 20 02:36:39 MSK 2011
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DA850/OMAP-L138/AM18xx EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci da850/omap-l138/am18xx variant 0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 8128
Kernel command line: mem=32M console=ttyS2,115200n8 root=/dev/mmcblk0p2 rw rootw
ait ip=off
PID hash table entries: 128 (order: -3, 512 bytes)
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory: 32MB = 32MB total
Memory: 28128KB available (3908K code, 263K data, 148K init, 0K highmem)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 149.50 BogoMIPS (lpj=747520)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 144 gpio irqs
regulator: core version 0.5
NET: Registered protocol family 16
MUX: initialized GPIO1_4
MUX: Setting register GPIO1_4
PINMUX4 (0x00000010) = 0x00222288 -> 0x00228288
MUX: initialized GPIO1_5
MUX: Setting register GPIO1_5
PINMUX4 (0x00000010) = 0x00228288 -> 0x00228888
da850_evm_init: HAS_MMC is enabled
MUX: initialized GPIO4_0
MUX: Setting register GPIO4_0
PINMUX10 (0x00000028) = 0x00222222 -> 0x80222222
MUX: initialized GPIO4_1
MUX: Setting register GPIO4_1
PINMUX10 (0x00000028) = 0x80222222 -> 0x88222222
MUX: initialized LCD_D_0
MUX: Setting register LCD_D_0
PINMUX17 (0x00000044) = 0x00000000 -> 0x00000020
MUX: initialized LCD_D_1
MUX: Setting register LCD_D_1
PINMUX17 (0x00000044) = 0x00000020 -> 0x00000022
MUX: initialized LCD_D_2
MUX: Setting register LCD_D_2
PINMUX16 (0x00000040) = 0x00000000 -> 0x20000000
MUX: initialized LCD_D_3
MUX: Setting register LCD_D_3
PINMUX16 (0x00000040) = 0x20000000 -> 0x22000000
MUX: initialized LCD_D_4
MUX: Setting register LCD_D_4
PINMUX16 (0x00000040) = 0x22000000 -> 0x22200000
MUX: initialized LCD_D_5
MUX: Setting register LCD_D_5
PINMUX16 (0x00000040) = 0x22200000 -> 0x22220000
MUX: initialized LCD_D_6
MUX: Setting register LCD_D_6
PINMUX16 (0x00000040) = 0x22220000 -> 0x22222000
MUX: initialized LCD_D_7
MUX: Setting register LCD_D_7
PINMUX16 (0x00000040) = 0x22222000 -> 0x22222200
MUX: initialized LCD_D_8
MUX: Setting register LCD_D_8
PINMUX18 (0x00000048) = 0x00000000 -> 0x00000020
MUX: initialized LCD_D_9
MUX: Setting register LCD_D_9
PINMUX18 (0x00000048) = 0x00000020 -> 0x00000022
MUX: initialized LCD_D_10
MUX: Setting register LCD_D_10
PINMUX17 (0x00000044) = 0x00000022 -> 0x20000022
MUX: initialized LCD_D_11
MUX: Setting register LCD_D_11
PINMUX17 (0x00000044) = 0x20000022 -> 0x22000022
MUX: initialized LCD_D_12
MUX: Setting register LCD_D_12
PINMUX17 (0x00000044) = 0x22000022 -> 0x22200022
MUX: initialized LCD_D_13
MUX: Setting register LCD_D_13
PINMUX17 (0x00000044) = 0x22200022 -> 0x22220022
MUX: initialized LCD_D_14
MUX: Setting register LCD_D_14
PINMUX17 (0x00000044) = 0x22220022 -> 0x22222022
MUX: initialized LCD_D_15
MUX: Setting register LCD_D_15
PINMUX17 (0x00000044) = 0x22222022 -> 0x22222222
MUX: initialized LCD_PCLK
MUX: Setting register LCD_PCLK
PINMUX18 (0x00000048) = 0x00000022 -> 0x02000022
MUX: initialized LCD_MCLK
MUX: Setting register LCD_MCLK
PINMUX18 (0x00000048) = 0x02000022 -> 0x22000022
MUX: initialized LCD_HSYNC
MUX: Setting register LCD_HSYNC
PINMUX19 (0x0000004c) = 0x00000000 -> 0x00000002
MUX: initialized LCD_VSYNC
MUX: Setting register LCD_VSYNC
PINMUX19 (0x0000004c) = 0x00000002 -> 0x00000022
MUX: initialized NLCD_AC_ENB_CS
MUX: Setting register NLCD_AC_ENB_CS
PINMUX19 (0x0000004c) = 0x00000022 -> 0x02000022
MUX: initialized GPIO2_8
MUX: Setting register GPIO2_8
PINMUX5 (0x00000014) = 0x00110110 -> 0x80110110
MUX: initialized GPIO2_15
MUX: Setting register GPIO2_15
PINMUX5 (0x00000014) = 0x80110110 -> 0x80110118
MUX: initialized RTC_ALARM
MUX: Setting register RTC_ALARM
PINMUX0 (0x00000000) = 0x44080000 -> 0x24080000
MUX: initialized GPIO2_4
MUX: Setting register GPIO2_4
PINMUX6 (0x00000018) = 0x00000000 -> 0x00008000
MUX: initialized GPIO6_13
MUX: Setting register GPIO6_13
PINMUX13 (0x00000034) = 0x00000000 -> 0x00000800
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Switching to clocksource timer0_1
musb_hdrc: version 6.0, cppi4.1-dma, peripheral, debug=0
Waiting for USB PHY clock good...
musb_hdrc: USB Peripheral mode controller at fee00000 using DMA, IRQ 58
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 1024 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
EMAC: MII PHY configured, RMII PHY will not be functional
MUX: initialized GPIO2_6
MUX: Setting register GPIO2_6
PINMUX6 (0x00000018) = 0x00008000 -> 0x00008080
NTFS driver 2.1.29 [Flags: R/W].
JFFS2 version 2.2. (NAND) В© 2001-2006 Red Hat, Inc.
JFS: nTxBlock = 219, nTxLock = 1758
msgmni has been set to 54
io scheduler noop registered (default)
da8xx_lcdc da8xx_lcdc.0: GLCD: Found Sharp_LK043T1DG01 panel
Console: switching to colour frame buffer device 60x34
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a 16550A
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a 16550A
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a 16550A
console [ttyS2] enabled
brd: module loaded
console [netcon0] enabled
netconsole: network logging started
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 1
ohci ohci.0: irq 59, io mem 0x01e25000
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
watchdog watchdog: heartbeat 60 sec
cpuidle: using governor ladder
cpuidle: using governor menu
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (439 buckets, 1756 max)
CONFIG_NF_CT_ACCT is deprecated and will be removed soon. Please use
nf_conntrack.acct=1 kernel parameter, acct=1 nf_conntrack module option or
sysctl net.netfilter.nf_conntrack_acct=1 to enable it.
xt_time: kernel timezone is -0000
IPv4 over IPv4 tunneling driver
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: (C) 2002 David S. Miller
TCP cubic registered
NET: Registered protocol family 17
Bridge firewalling registered
Clocks: disable unused i2c1
Clocks: disable unused emac
Clocks: disable unused mcasp
Clocks: disable unused aemif
Clocks: disable unused spi0
Clocks: disable unused spi1
Clocks: disable unused mcbsp0
Clocks: disable unused mcbsp1
Clocks: disable unused vpif
------------[ cut here ]------------
WARNING: at arch/arm/mach-davinci/da850.c:1178 da850_regulator_init+0x3c/0x58()
Unable to obtain voltage regulator for CVDD; voltage scaling unsupported
Modules linked in:
Backtrace:
[<c0031730>] (dump_backtrace+0x0/0x114) from [<c0321220>] (dump_stack+0x18/0x1c)
r7:c1c23d40 r6:c0039540 r5:c03a7b16 r4:0000049a
[<c0321208>] (dump_stack+0x0/0x1c) from [<c0041b8c>] (warn_slowpath_common+0x50/
0x68)
[<c0041b3c>] (warn_slowpath_common+0x0/0x68) from [<c0041bf0>] (warn_slowpath_fm
t+0x30/0x38)
r7:c1d68c00 r6:c043936c r5:c0404280 r4:c0420ccc
[<c0041bc0>] (warn_slowpath_fmt+0x0/0x38) from [<c0039540>] (da850_regulator_ini
t+0x3c/0x58)
r3:c0411cac r2:c03a7b34
[<c0039504>] (da850_regulator_init+0x0/0x58) from [<c000f70c>] (davinci_cpu_init
+0x40/0xc0)
r5:c0404280 r4:c1dd2300
[<c000f6cc>] (davinci_cpu_init+0x0/0xc0) from [<c0257a94>] (cpufreq_add_dev+0x15
4/0x41c)
r5:c1dd2300 r4:00000000
[<c0257940>] (cpufreq_add_dev+0x0/0x41c) from [<c020683c>] (sysdev_driver_regist
er+0xb8/0x128)
[<c0206784>] (sysdev_driver_register+0x0/0x128) from [<c0256ba8>] (cpufreq_regis
ter_driver+0xf4/0x1a0)
r6:c0406074 r5:c0402d90 r4:c0420cfc
[<c0256ab4>] (cpufreq_register_driver+0x0/0x1a0) from [<c000f6ac>] (davinci_cpuf
req_probe+0x90/0xb0)
r5:c0402d90 r4:c0420cfc
[<c000f61c>] (davinci_cpufreq_probe+0x0/0xb0) from [<c0208f20>] (platform_drv_pr
obe+0x20/0x24)
r5:c04034b0 r4:c04034b0
[<c0208f00>] (platform_drv_probe+0x0/0x24) from [<c0207f44>] (driver_probe_devic
e+0xb0/0x164)
[<c0207e94>] (driver_probe_device+0x0/0x164) from [<c0208060>] (__driver_attach+
0x68/0x8c)
r7:c1d68c00 r6:c0406074 r5:c04034e4 r4:c04034b0
[<c0207ff8>] (__driver_attach+0x0/0x8c) from [<c0207704>] (bus_for_each_dev+0x50
/0x84)
r7:c1d68c00 r6:c0406074 r5:c0207ff8 r4:00000000
[<c02076b4>] (bus_for_each_dev+0x0/0x84) from [<c0207da8>] (driver_attach+0x20/0
x28)
r6:c0406074 r5:c0406074 r4:c0024d34
[<c0207d88>] (driver_attach+0x0/0x28) from [<c0206fdc>] (bus_add_driver+0xa4/0x2
30)
[<c0206f38>] (bus_add_driver+0x0/0x230) from [<c020837c>] (driver_register+0xb0/
0x13c)
[<c02082cc>] (driver_register+0x0/0x13c) from [<c020938c>] (platform_driver_regi
ster+0x4c/0x60)
r9:00000000 r8:00000000 r7:00000001 r6:c000f5f8 r5:c0406060
r4:c0024d34
[<c0209340>] (platform_driver_register+0x0/0x60) from [<c02093c0>] (platform_dri
ver_probe+0x20/0xb4)
[<c02093a0>] (platform_driver_probe+0x0/0xb4) from [<c000f610>] (davinci_cpufreq
_init+0x18/0x24)
r7:00000001 r6:c000f5f8 r5:00000000 r4:c0024d34
[<c000f5f8>] (davinci_cpufreq_init+0x0/0x24) from [<c002d3a4>] (do_one_initcall+
0x64/0x1c4)
[<c002d340>] (do_one_initcall+0x0/0x1c4) from [<c0008480>] (kernel_init+0xa8/0x1
2c)
r7:00000000 r6:00000000 r5:00000000 r4:c0024d34
[<c00083d8>] (kernel_init+0x0/0x12c) from [<c00454a4>] (do_exit+0x0/0x6b4)
r5:00000000 r4:00000000
---[ end trace 10fdf51caa867526 ]---
davinci_emac_probe: using random MAC addr: 66:a0:a2:27:c3:0d
emac-mii: probed
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
Waiting for root device /dev/mmcblk0p2...