This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA829J: Set module clock parent via direct registers access

Part Number: DRA829J

Tool/software:

Dear TI-Team,

Clocks with the name _PARENT_ are not directly fed to the module but feed into a multiplexer and then based on the value of the multiplexer will reach the module.
See FAQ: https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/07_03_00_07/exports/docs/pdk_jacinto_07_03_00_29/docs/userguide/jacinto/faq/faq_module_clocking.html

However, we want to avoid the usage of Sciclient_pmSetModuleClkParent function to select the value of the multiplexer. We would rather write it directly to the MMR register (CLK_SEL bitfield).

Assuming that PLL configuration is already done and frequency is correct, do we need to take into consideration any additional steps to select the source clock? (e.g. trigger RST)

If you have a procedure (including additional steps) to change clock parent with detailed description would be perfect.

Thank you in advance.
António

  • Hi Antonio,

    However, we want to avoid the usage of Sciclient_pmSetModuleClkParent function to select the value of the multiplexer. We would rather write it directly to the MMR register (CLK_SEL bitfield).

    Why do you want to do this, what are your reasons?

    Also, what core are you trying to set this from, and for what peripheral?

    If you have a procedure (including additional steps) to change clock parent with detailed description would be perfect.

    No, there is no ready-made procedure available for this in the SDK, 

    The TDA4 devices are heterogenous devices with multiple processors, and all Clock and Device Management is centralized under the SciServer managed by the MCU1_0 core.  Some of the mux clocks do drive multiple peripherals, and if you are trying to modify registers directly, then the SoC could hang-up due to incorrect configurations, and mismatched state machine logic. 

    regards

    Suman

  • Hi Suman
    Thanks for your quick response.

    Why do you want to do this, what are your reasons?

    Also, what core are you trying to set this from, and for what peripheral?

    We are working on a very specific project that requires avoiding the use of Sciclient functions. The goal is to minimize dependencies on the M3 core as much as possible. As a result, we are rewriting all functions related to board configuration.

    This configuration is performed by SBL (our costum bootloader) running on the MCU Core and affects all peripherals that we plan to use.

    The TDA4 devices are heterogenous devices with multiple processors, and all Clock and Device Management is centralized under the SciServer managed by the MCU1_0 core.  Some of the mux clocks do drive multiple peripherals, and if you are trying to modify registers directly, then the SoC could hang-up due to incorrect configurations, and mismatched state machine logic.

    We are aware of it. Nevertheless, we would like to confirm whether SciServer performs any additional actions or verifications when setting the new mux value (besides confirming that frequency is correct).

    Here is an overview of the sequence we have implemented:
    1. Configure PLLs and set desired frequencies
    2. Configure source clocks by setting mux values via direct register access (CLK_SEL bitfield)
    3. Power configuration (setting PDs and LPSCs)

    Knowing this, do we need to take into consideration any additional steps to select the source clock? (e.g. trigger RST)

    Thank you.
    António

  • Hi Antonio,

    We are working on a very specific project that requires avoiding the use of Sciclient functions.

    What end-equipment market is your project/product geared towards?

    I still do not see the reasons other than your preference to avoid this. Are you planning not to use the Sciclient library at all? If so, is your usage going to be different between SBL and when the MCU1_0 application is running.

    The goal is to minimize dependencies on the M3 core as much as possible. As a result, we are rewriting all functions related to board configuration.

    The TIFS (DMSC M3) core is very fundamental to the overall Device Boot, and this core needs to be booted before you can proceed further on the overall boot. The TIFS firmware handles all the Security related configuration - including processor boot and firewall configuration. So, you cannot even boot other cores without the TIFS M3 core.

    The Board Configuration is used by both the TIFS cores (TIFS firmware becomes ready only after processing these requests), and the MCU1_0 SciServer/Device Management code for the SciClient interface.

    Please note that TIFS firmware sets up some initial firewalls as well during its boot covering some of the relevant register regions. Please see J721E Firewall Descriptions for a list of registers covered.

    This configuration is performed by SBL (our costum bootloader) running on the MCU Core and affects all peripherals that we plan to use.

    The overall Clock and PSC configuration is actually owned by the MCU1_0 firmware, and both SBL and MCU1_0 firmwares do use the Sciclient_direct library, which are native library calls on MCU1_0. The Sciclient library is a wrapper here over the lower-level functions implemented within the rm_pm_hal library code.

    Here is an overview of the sequence we have implemented:
    1. Configure PLLs and set desired frequencies
    2. Configure source clocks by setting mux values via direct register access (CLK_SEL bitfield)
    3. Power configuration (setting PDs and LPSCs)

    Knowing this, do we need to take into consideration any additional steps to select the source clock? (e.g. trigger RST)

    PLLs are already configured with default frequencies during Sciclient_init within SBL code. Please note that both ROM and TIFS does configure some PLLs as well during their boot, and rest of the PLLs are initialized during the Sciclient initialization within SBL code.

    Anyway, these are the same steps that would have been done by SBL within Sciclient_init and any specific source selection. The Power Configuration is the only piece that is handled within each driver as part of init (they all use the Sciclient API).

    What all layers are you rewriting overall?

    regards

    Suman

  • Hi Suman

    Please find my answers below. Note that we have developed our own SBL where board configuration is done.

    What end-equipment market is your project/product geared towards?

    It is for Aerospace market.

    Are you planning not to use the Sciclient library at all?

    Yes, we want to avoid that dependence.

    What all layers are you rewriting overall?

    Besides TIFS (mandatory to boot), we are planning to rewrite everything else.
    Therefore, the goal is to minimize dependencies on the M3 core as much as possible.
    For this reason we need to confirm correctness of the clock changing procedure to implement on our custom SBL.

    So, do you know whether we need to consider extra steps when selecting source clock (besides selecting mux value)?

    Thank you.
    António

  • Hi Antonio,

    The engineer responsible is currently out of office. Please expect 4 business day delay in response.

    Regards,

    Takuma

  • Hi Antonio,

    It is for Aerospace market.

    Ok, thanks for the clarifications. I understand the reasons/needs for this given that this is for Aerospace market.

    Yes, we want to avoid that dependence.

    Are there any parts of the Sciclient layers that you would re-use? Sciclient_direct is a wrapper library over the low-level rm_pm_hal drivers.

    Besides TIFS (mandatory to boot), we are planning to rewrite everything else.

    OK, the SoC has lot of clocks and device information. So, will you be rewriting even the device and clock data as well?

    The PLL initialization sequence for example needs to be written very carefully if you are going to rewrite the PLL driver code yourself as well.

    TI can only provide generic guidance, and won't be able to provide any debug support for issues that that may be introduced in your code.

    Therefore, the goal is to minimize dependencies on the M3 core as much as possible.

    The TIFS boot still requires that the board configuration data be passed to it, without which it is not in a functionally ready-state. You would need this at the minimum, for supporting

    I don't know what your s/w dependencies are for configuring firewalls, or using UDMA between multiple cores. Any firewall setup and processor boot sequences will require the M3 core for sure. Will you be using a GP device or a HS device, and if latter, is this going to be a HS-Prime device (that may allow you to customize TIFS firmware)?

    So, do you know whether we need to consider extra steps when selecting source clock (besides selecting mux value)?

    The Mux selection registers in CTRL_MMR registers may require you to unlock the partition to allow-writing in general. A dedicated peripheral clock selection probably is a simpler change, but you need to be careful with changing PLLs or the PLL Divider Clocks, since they can supply more than one peripheral with different clocking requirements. 

    regards

    Suman

  • Hi Suman

    Are there any parts of the Sciclient layers that you would re-use? Sciclient_direct is a wrapper library over the low-level rm_pm_hal drivers.

    Due to DO-178 certification we need to avoid their usage.

    OK, the SoC has lot of clocks and device information. So, will you be rewriting even the device and clock data as well?

    The PLL initialization sequence for example needs to be written very carefully if you are going to rewrite the PLL driver code yourself as well.

    TI can only provide generic guidance, and won't be able to provide any debug support for issues that that may be introduced in your code.

    We are aware of that. We have already re-written most of the code.
    PLL initialization is implemented and working.

    The TIFS boot still requires that the board configuration data be passed to it, without which it is not in a functionally ready-state. You would need this at the minimum, for supporting

    This is under analysis. We are passing the current TI configuration. But in the near future we need to understand which is the minimal configuration needed/passed by/to TIFS.

    I don't know what your s/w dependencies are for configuring firewalls, or using UDMA between multiple cores. Any firewall setup and processor boot sequences will require the M3 core for sure. Will you be using a GP device or a HS device, and if latter, is this going to be a HS-Prime device (that may allow you to customize TIFS firmware)?

    It will be used as GP device.

    A dedicated peripheral clock selection probably is a simpler change

    Does it mean we don't need any additional step to select a dedicated clock source? Setting mux value is enough and safe?

    but you need to be careful with changing PLLs or the PLL Divider Clocks, since they can supply more than one peripheral with different clocking requirements. 

    Yes correct. We take into consideration this limitation while performing PLL initialization.


    So, can you confirm the question regarding clock selection please?

    Thank you.
    António

  • Hi Antonio,

    Due to DO-178 certification we need to avoid their usage.

    Ok. I understand that this is the Safety certification standard in Aerospace industry at high-level, but am not what it entails in general or what extra details it requires when compared to the Automotive ISO-26262 standard (which is what our RTOS s/w is written for in general).

    This is under analysis. We are passing the current TI configuration. But in the near future we need to understand which is the minimal configuration needed/passed by/to TIFS.

    The main variability is around the RM Board Configuration data, again it would mostly be around how you need to deal with DMA channel separation between different processing cores.

    It will be used as GP device.

    Ok. TIFS will still setup the initial firewalls as per J721E Firewall Descriptions even on a GP device.

    Does it mean we don't need any additional step to select a dedicated clock source? Setting mux value is enough and safe?

    Yes, as long as that mux clock is not driving mutiple peripherals, it would be as simple as that. Hopefully, you would have configured the desired clock rates on the parent clocks as all needed.

    Again, given that this is all your implementation and zero re-use from TI clock data, it all depends on how you are dealing with all the leaf clocks.

    regards

    Suman

  • Hi Suman,
    Thanks for you reply.

    as long as that mux clock is not driving mutiple peripherals,

    However, I'm not entirely clear on this condition. What do you actually mean?
    And what could be the impact?

    Thank you.
    António

  • Hi Antonio,

    However, I'm not entirely clear on this condition. What do you actually mean?

    This is a question of the distribution of Clocks (You can easily see this with PLL HSDIV clocks for example).

    If this said clock is driving two different peripherals, then you would need to be using an aligned frequency that both the peripherals can use.

    And what could be the impact?

    You cannot unilaterally change for one peripheral and expect the other peripheral to continue to work properly.

    regards

    Suman

  • Hi Suman,
    Thanks for your clarification.

    then you would need to be using an aligned frequency that both the peripherals can use

    We are aware of this frequency alignment.
    Our main concern is about the clock source selection through direct register access (mux value).

    If you confirm that there's no other risk besides frequency alignment, then we can close this thread.

    Thank you.
    António

  • Hi Antonio,

    Our main concern is about the clock source selection through direct register access (mux value).

    Yes, no issues around that. The low-level clock driver within the rm_pm_hal library does exactly the same.

    If you confirm that there's no other risk besides frequency alignment, then we can close this thread.

    Yeah, no other concerns. 

    Do follow the locking and unlocking of the CTRL_MMR registers so that there are no accidental writes. 

    Closing the thread.

    regards

    Suman