This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: Video flickering on IMX335 camera

Part Number: SK-AM62A-LP


Tool/software:

Hello Engineer,

I am tried to use IMX335 5MP USB camera with SK-AM62A. When running the apps_python application, It seems flickering in the output video.

When I move approximate nearer (less than 15 cm) or check by placing an object nearer to camera disappears this issue, exist in saved video also. Tried changing the input and output frame rate also, but no change in the out.

Warm Regards,
Sajan

  • Hi Sajan,

    Would you mind sharing a video showing the flickering?

    Thank you.

    Jianzhong

  • Hello Jianzhong,

    Would you mind sharing a video showing the flickering?

    Here is the video



    Warm Regards,
    Sajan

  • Hi Sajan,

    You're not using the ISP on AM62A, right?

    Can you run a simple Gstreamer command to stream the camera to a display and see if flickering is there? I'd like to narrow down the problem.

    Thank you.

    Jianzhong

  • Hello Jianzhong,

    You're not using the ISP on AM62A, right?

    This video is using in built ISP and video is saved from apps_python.

    Warm Regards,
    Sajan

  • Sajan,

    Can you use Gstreamer to save video to a file and share it here?

    Thank you.

    Jianzhong