Part Number: TDA4AL-Q1
Tool/software:
Hi all
we use tda4al with custom baord.
If the debug UART is changed from UART8 to UART5 on a custom board, which files need to be modified?
BR
liupt
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4AL-Q1
Tool/software:
Hi all
we use tda4al with custom baord.
If the debug UART is changed from UART8 to UART5 on a custom board, which files need to be modified?
BR
liupt
hello all
We use sdk 11.
Additional question: The EVM board has 16GB DDR, but the custom board only has 8GB (same DDR model). Where do I need to make modifications?
BR
liupt
Hi Peitao,
Are you using linux or RTOS?
Which is the SDK version you are using?
Regards
Gokul
HI GoKul
We use sdk11 & SPL linux&rtos
I had modify those files.
psdkla/board-support/ti-u-boot-2025.01+git/dts/upstream/src/arm64/ti/k3-j721s2-common-proc-board.dts
serial2 = &main_uart5;
psdkla/board-support/ti-u-boot-2025.01+git/arch/arm/dts/k3-j721s2-common-proc-board-u-boot.dtsi
-&main_uart8_pins_default {
- bootph-all;
-&main_uart8 {
- bootph-all;
-};
+&uart5_pins_default {
+ bootph-all;
+
+&main_uart5 {
+ bootph-all;
+};
psdkra/app_utils/utils/misc/src/app_pinmux_j721s2.c
add
static pinmuxPerCfg_t gUart5PinCfg[] =
{
/* UART5 -> UART5_RXD -> AC24 */
{
PIN_MCAN12_RX, PIN_MODE(11) | \
((PIN_PULL_DISABLE | PIN_INPUT_ENABLE) & (~PIN_PULL_DIRECTION))
},
/* UART5 -> UART5_TXD -> W25 */
{
PIN_MCAN12_TX, PIN_MODE(11) | \
((PIN_PULL_DISABLE | PIN_INPUT_ENABLE) & (~PIN_PULL_DIRECTION))
{PINMUX_END}
};
psdkla/board-support/ti-u-boot-2025.01+git/doc/board/ti/j721s2_evm.rst
export TFA_EXTRA_ARGS="K3_USART=0x8"---》export TFA_EXTRA_ARGS="K3_USART=0x5"
export OPTEE_EXTRA_ARGS="CFG_CONSOLE_UART=0x8" ---》export OPTEE_EXTRA_ARGS="CFG_CONSOLE_UART=0x5"
Previously, when there was a DDR issue, logs would be output(
).
However, after modifying the DDR configuration, there are no logs at all.
thank you
BR
liupt
Hi Gokul
I made the following modification:
+++ b/psdkla/board-support/trusted-firmware-a-2.12+git/plat/ti/k3/include/platform_def.h
@@ -90,7 +90,7 @@
/* Platform default console definitions */
#ifndef K3_USART_BASE
-#define K3_USART_BASE (0x02800000 + 0x10000 * K3_USART)
+#define K3_USART_BASE (0x28850000 + 0x10000 * K3_USART)
Now the serial port outputs logs after power-on:
U-Boot SPL 2025.01-ti (Aug 20 2025 - 17:09:45 +0800)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.9--v11.00.09+ (Fancy Rat)')
SPL initial stack usage: 13456 bytes
Trying to boot from MMC2
Skipping authentication on GP device
Skipping authentication on GP device
Skipping authentication on GP device
Skipping authentication on GP device
Skipping authentication on GP device
Loading Environment from nowhere... OK
Starting ATF on ARM64 core...
Then got stuck, what else do I need to change?
BR
liupt