Hi,
Lately,I encounted two problems when I test the encoder/decoder applied by TI for DM6467T. The encoder/decoder's version are follow,
h264enc 01.20.02.00
h264dec 01.10.05.05
h264fhdvenc 01.10.02.05
h2641080p60vdec 01.20.00.14
One problem is that h264fhdvenc's releasenotes write like this
SDOCM00057668 Simultaneous encode + decode not supported because both HDVICPS are used by the 1080p encoder DM6467_BP_001
but no similar description for 720p. And The programm went to deadlock when I tested Simultaneous encode + decode for 720p. So I cann't conform whether the encoder h264fhdvenc supports simultaneous encode + decode for 720p.
The other problem is that h264enc's UserGuide write like this
Supports limited High Profile with 8x8 transforms for Intra Macro Blocks
I set "EntropyCodingMode = 1; profileIdc = 100; videncDynamicParams.targetBitRate = 512000;"
But, the image effect is no better than BP(profileIdc = 66).
So, how can I set the params If I want to use the high profile function and get better image effect ?
Thanks for anybody giving me the answers.
Best regards,
LiuLiang