Tool/software:
I want to know host's USB 2.0(FULL-Speed) compliance tests commands on a board equipped with DRA821-Q1.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I want to know host's USB 2.0(FULL-Speed) compliance tests commands on a board equipped with DRA821-Q1.
HI HYUKJUN,
I have redirected this query to corresponding expert. Thanks in advance for your patience.
Regards
Gokul
HYUKJUN,
I have not performed the FS mode compliance tests since they are at lower speeds compared to the HS test mode; but my suggestion would be to first put the SoC into the FS mode and then enable the test pattern through the same field as HS. You could also use the USB-IF tool and select to put out the test packet at the DP/DM data pins.
Thank you for your reply.
First, just to confirm, is there no command to send a host FS mode test packet?
Also, I'd like more specific information about the method you suggested.
How do I switch the SoC to FS mode?
Is the following the correct command to enter after switching to FS mode?
devmem2 0x06010480 w 0x000000A0
devmem2 0x06010080 w 0x00000004
devmem2 0x06010484 w 0x40000000
I'd like to perform a host-side compliance test.
Is there a way to output test packets on the DP/DM data pins using the USB-IF tool?
Thank you in advance.
Hyukjun,
Yes, for the host-side compliance test, these are the commands to output the compliance test packet.
06020000h[13] can be set to 1 to enable FS mode.