Hi all,
I use blaze 4430 ES2.2 board, and remove the LCD panel. I can't get the HDMI work with Android 4.0. I follow omappedia to build u-boot, xloader, kernel and ASF file.
http://www.omappedia.org/wiki/L27.IS.1_OMAP4_Icecream_Sandwich_Release_Notes
The kernel can't setup framebuff. How to make the HDMI work when there is no other VIDEO devices?
<7>[ 5.272766] omapdss OVERLAY: check_overlay 0: (0,0 640x480 -> 640x480) disp (640x480)
<7>[ 5.281311] omapdss MANAGER: omap_dss_mgr_apply(lcd)
<6>[ 5.286712] cannot apply mgr(lcd) on inactive device
<4>[ 5.292022] omapfb omapfb: failed to apply dispc config
<7>[ 5.297607] omapdss MANAGER: omap_dss_mgr_apply(tv)
<7>[ 5.302764] omapdss OVERLAY: check_overlay 0: (0,0 640x480 -> 640x480) disp (640x480)
<7>[ 5.311065] omapdss MANAGER: configure_overlay(0)
<7>[ 5.316070] omapdss DISPC: dispc_setup_plane 0, pa a9a00000, sw 640, 0,0, 640/1x480/1 -> 640x480, ilace 0, cmode 800, rot 0, mir 0 chan 1 3tap
<7>[ 5.329620] omapdss DISPC: calc_rot(0): scrw 640, 640x480
<7>[ 5.335327] omapdss DISPC: offset0 0, offset1 0, row_inc 1, pix_inc 1
<7>[ 5.342132] omapdss DISPC: 0,0 640*1x480*1 -> 640x480
<7>[ 5.347503] omapdss DISPC: fifo(0) low/high old 1272/1279, new 944/1279
<7>[ 5.354492] omapdss DISPC: dispc_enable_plane 0, 1
<7>[ 5.359558] omapdss MANAGER: configure_manager(1)
<7>[ 5.364562] omapdss DISPC: GO DIGIT
<7>[ 5.368286] omapdss MANAGER: omap_dss_mgr_apply(lcd2)
<6>[ 5.373657] cannot apply mgr(lcd2) on inactive device
<4>[ 5.378997] omapfb omapfb: failed to apply dispc config
<7>[ 5.384552] omapdss: ENTER hdmi_panel_enable
<4>[ 5.389068] omapfb omapfb: Failed to enable display 'hdmi'
<3>[ 5.394897] omapfb omapfb: failed to initialize default display
<7>[ 5.402587] omapdss MANAGER: omap_dss_mgr_blank(tv,wait=1)
<7>[ 5.408416] omapdss MANAGER: configure_overlay(0)
<7>[ 5.413391] omapdss DISPC: dispc_enable_plane 0, 0
<7>[ 5.418457] omapdss MANAGER: configure_overlay(1)
<7>[ 5.423431] omapdss DISPC: dispc_enable_plane 1, 0
<7>[ 5.428497] omapdss MANAGER: configure_overlay(2)
<7>[ 5.433471] omapdss DISPC: dispc_enable_plane 2, 0
<7>[ 5.438537] omapdss MANAGER: configure_overlay(3)
<7>[ 5.443511] omapdss DISPC: dispc_enable_plane 3, 0
<7>[ 5.448608] omapdss MANAGER: configure_manager(1)
<7>[ 5.453582] omapdss DISPC: GO DIGIT
<6>[ 5.465118] omapdss HDMI: Enter hdmi_display_disable
<6>[ 5.478546] omapdss HDMI: Release c-state constraint for HDMI
<6>[ 5.478546]
<7>[ 5.486206] omapdss HDMI: hdmi_runtime_put
<7>[ 5.490570] omapdss DISPC: dispc_runtime_put
<7>[ 5.495086] omapdss DISPC: dispc_save_context
<7>[ 5.499969] omapdss DISPC: context saved, ctx_loss_count -2
<7>[ 5.505950] omapdss DSS: dss_runtime_put
<7>[ 5.510101] omapdss DSS: dss_save_context
<7>[ 5.514373] omapdss DSS: context saved
<6>[ 5.518371] hdmi: clearing EDID info
<3>[ 5.522186] omapfb omapfb: failed to setup omapfb
<4>[ 5.527191] omapfb: probe of omapfb failed with error -22
<3>[ 5.534820] omaplfb: OMAPLFB_Init: OMAPLFBInit failed