This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Android2.3.4 DSP porting

HI:

  I want to port DSP to the android2.3.4

  I check the harware/ti have the following directories

   am45x  omap3  sgx  wlan  wpan


  No directory "omap" there. In this directory ,video audio libraries are built.

  but I can find "omap" on androird2.3 or froyo.

  This means I should set HARDWARE_OMX to use dspbridge in the BoardConfig.mk?

  But TI just release dvsdk_dm3730-evm_04_03_00_06_setuplinux on 2011/12/23.

  I can build the drivers. but these drivers must be used with libraries in the omap.

  Can I copy "omap" directory from android2.3.

  My question is

  which shoild I use(HARDWARE_OMX or dvsdk_dm3730-evm_04_03_00_06_setuplinux) ? and how to get omap directory?