hi
am working Devkit8000 board, has OMAP 3530. NAND flash memory of 256 MB is availabe.
am loading Angstrom OS in NAND flash and every thing is working fine.
0x00000000-0x00080000 : "X-Loader"
0x00080000-0x00260000 : "U-Boot"
0x00260000-0x00280000 : "U-Boot Env"
0x00280000-0x00680000 : "Kernel"
0x00680000-0x10000000 : "File System"
here i am utilizing only few MB of memry for Anstrom OS.
Problem is i have created one more extra partition see below
0x00000000-0x00080000 : "X-Loader"
0x00080000-0x00260000 : "U-Boot"
0x00260000-0x00280000 : "U-Boot Env"
0x00280000-0x00680000 : "Kernel"
0x00680000-0x01940000 : "File System"
0x01940000-0x10000000 : "EXTENDED PARTITION"
when booting i am getting an error
UBIFS error (pid 1): ubifs_get_sb: cannot open "ubi0:rootfs", error -19
VFS: Cannot open root device "ubi0:rootfs" or unknown-block(0,0)
Please append a correct "root=" boot option; here are the available partitions:
1f00 131072 mtdblock0 (driver?)
1f01 512 mtdblock1 (driver?)
1f02 1920 mtdblock2 (driver?)
1f03 128 mtdblock3 (driver?)
1f04 4096 mtdblock4 (driver?)
1f05 19200 mtdblock5 (driver?)
1f06 236288 mtdblock6 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
FOR COMPLETE REFERENCE PLEASE REFER THE FILE minicom_output.txt
please suggest me how rectify this problem
thanks and regards
N REDDY0044.minicom_output.txt