This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Query in Reset and Power supply monitoring section

Other Parts Discussed in Thread: TMS320DM8168

Respected Sir,

                               In the EVM of TMS320DM8168, TPS3808G09DBVRG4 is used which has Reset Threshold voltage of 0.84V. Instead I have used TPS3823-33 with the supply voltage 3.3V and it has Reset Threshold of min 2.88V to max 3V. Will this logic work properly? Or is there any specific reason to use TPS3808G09 IC?

                              Thank you,