This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CPU usage too high while accessing SD card

Hello,

I try to test SD card performance by following command,

time sh -c "dd if=/dev/zero of=/mnt/mmc/ddfile bs=1M count=100 ; sync"

But, it cause CPU usage is around 40%.


I have same issue like following link

http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/t/84931.aspx

But, the patch is using 2.6.18, does anyone has patch file which is based on 2.6.32?

Thanks,

Thomas.