Part Number: AM623
Tool/software:
MCU SDK 10. 0.0.14 released on Aug 14.2025

Linux SDK10.0.07.04 release on the same day Aug. 14.2025, but its ti-firmware mc sdk version is 10.0.0.8, not 10.0.0.14.

Now customer need to modify something base on MCU SDK 10.0.08.
Find source code from here, follow the README.md,
https://github.com/TexasInstruments/mcupsdk-core-k3/blob/REL.MCUSDK.K3.10.00.00.08/README.md
get error on repo sync
tony@ubuntu22:~$ sudo apt-get update [sudo] password for tony: Hit:1 http://us.archive.ubuntu.com/ubuntu jammy InRelease Get:2 http://us.archive.ubuntu.com/ubuntu jammy-updates InRelease [128 kB] Get:3 http://us.archive.ubuntu.com/ubuntu jammy-backports InRelease [127 kB] Get:4 http://us.archive.ubuntu.com/ubuntu jammy-security InRelease [129 kB] Fetched 384 kB in 6s (67.4 kB/s) Reading package lists... Done tony@ubuntu22:~$ sudo apt-get install repo Reading package lists... Done Building dependency tree... Done Reading state information... Done repo is already the newest version (2.17.3-3). The following packages were automatically installed and are no longer required: linux-headers-5.15.0-140 linux-headers-5.15.0-140-generic linux-headers-5.15.0-141 linux-headers-5.15.0-141-generic linux-headers-5.15.0-143 linux-headers-5.15.0-143-generic linux-image-5.15.0-140-generic linux-image-5.15.0-141-generic linux-image-5.15.0-143-generic linux-modules-5.15.0-140-generic linux-modules-5.15.0-141-generic linux-modules-5.15.0-143-generic linux-modules-extra-5.15.0-140-generic linux-modules-extra-5.15.0-141-generic linux-modules-extra-5.15.0-143-generic Use 'sudo apt autoremove' to remove them. 0 upgraded, 0 newly installed, 0 to remove and 76 not upgraded. tony@ubuntu22:~$ tony@ubuntu22:~$ repo init -u https://github.com/TexasInstruments/mcupsdk-manifests.git -m am62x/dev.xml -b k3_main repo: reusing existing repo client checkout in /home/tony repo has been initialized in /home/tony tony@ubuntu22:~$ tony@ubuntu22:~$ repo init -u https://github.com/TexasInstruments/mcupsdk-manifests.git -m am62x/main.xml -b k3_main repo: reusing existing repo client checkout in /home/tony repo has been initialized in /home/tony tony@ubuntu22:~$ tony@ubuntu22:~$ repo sync Syncing: 13% (2/15), done in 10.451s fatal: couldn't find remote ref refs/tags/DEV.MCUSDK.K3.11.01.00.20 trusted-firmware-a: fatal: couldn't find remote ref refs/tags/DEV.MCUSDK.K3.11.01.00.20 trusted-firmware-a: sleeping 4.0 seconds before retrying fatal: couldn't find remote ref refs/tags/DEV.MCUSDK.K3.11.01.00.20 fatal: couldn't find remote ref refs/tags/DEV.MCUSDK.K3.11.01.00.20 proc-ospi-tuning: fatal: couldn't find remote ref refs/tags/DEV.MCUSDK.K3.11.01.00.20 proc-ospi-tuning: sleeping 4.0 seconds before retrying fatal: couldn't find remote ref refs/tags/DEV.MCUSDK.K3.11.01.00.20 Syncing: 100% (15/15) 0:27 | 2 jobs | 0:06 mbedtls @ mcu_plus_sdk/source/networking/mbedtls..error: Unable to fully sync the tree error: Downloading network changes failed. Failing repos (network): mcu_plus_sdk/source/atf/trusted-firmware-a mcu_plus_sdk/source/drivers/ospi/v0/ospi_tuning Try re-running with "-j1 --fail-fast" to exit at the first error. ================================================================================ Repo command failed due to the following `SyncError` errors: GitCommandError: 'fetch --quiet --progress atf --prune --recurse-submodules=no --tags +refs/heads/*:refs/remotes/atf/* +refs/tags/DEV.MCUSDK.K3.11.01.00.20:refs/tags/DEV.MCUSDK.K3.11.01.00.20 +refs/tags/*:refs/tags/*' on trusted-firmware-a failed stdout: fatal: couldn't find remote ref refs/tags/DEV.MCUSDK.K3.11.01.00.20 GitCommandError: 'fetch --quiet --progress origin --prune --recurse-submodules=no --tags +refs/heads/*:refs/remotes/origin/* +refs/tags/DEV.MCUSDK.K3.11.01.00.20:refs/tags/DEV.MCUSDK.K3.11.01.00.20 +refs/tags/*:refs/tags/*' on proc-ospi-tuning failed stdout: fatal: couldn't find remote ref refs/tags/DEV.MCUSDK.K3.11.01.00.20 tony@ubuntu22:~$
Support needs: build MCU+ SDK10.0.0.8