This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADB via USB on Netra (DM816xEVM)



Hi all

Can any one help me to enable ADB over USB on NETRA(DM816xevm).

I have followed link below:
http://processors.wiki.ti.com/index.php/Usbgeneralpage#One_port_as_host_and_other_port_as_Gadget_.28for_DM81XX.29

I have followed the below steps:

1. make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi- distclean
2. make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi- ti8168_evm_defconfig
3. make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi- menuconfig

but in menuconfig I am unable find following configuration lines as given in the link

TI816X usb connector's ID pin control (from software setting)  --->
                            Force TI816X USB0 to  (Host mode)  --->
                            Force TI816X USB1 to  (Host mode)  --->