Other Parts Discussed in Thread: TAD5212, SYSCONFIG
Tool/software:
I made a change syscfg file to use MCASP2, but TDM communication waveform cannot be verified from AEC2 (Audio Expansion Connector)
I'm developing based on AM275-AWE-SDK_11.00.00.17.
It is known that this SDK realizes 8 channel input and output through MCASP1 by receiving TDM8 from two AD converters (PCM6240) and transmitting TDM8 to four DA converters (TAD5212).
What is the correct change to the syscfg file?
Is AEC tested?
If AEC2 is being tested, is the test environment shareable?