Part Number: AM67
Tool/software:
Hi
I was following the TI official guideline to install sdk and load a prebuilt image on the SD card.
Here is my workflow could you help me review if anything wrong steps that will cause the EVM can't boot up?
Enviroment
Ubuntu 22.04
Device: xj722s5a amw(am67 EVM)
Build & Load image step
- sudo -s
- install sdk under /opt/
- ./setup.sh
- make
- make linux
- cd bin
- ./create-sdcard.sh(the sd card include root and boot pattion
i try using command line and also balena to create sd card
And the image i use : tisdk-default-image-j722s-evm.rootfs.tar.xz - use pinconcom
- sudo picocom -b 115200 -r -l /dev/ttyUSB0(to see the log and it stuck in the boot flow
it's keep repeat the first inital didn't enter to next step
And i double check the boot folder include tiboot3.bin/ tispl.bin / u-boot.img
-----------------------
error log
seamus@Linux-PC:/opt/ti-processor-sdk-linux-am67-sk-11_00_10_01/board-support/prebuilt-images$ sudo picocom -b 115200 -r -l /dev/ttyUSB0
[sudo] password for seamus:
picocom v3.1
port is : /dev/ttyUSB0
flowcontrol : none
baudrate is : 115200
parity is : none
databits are : 8
stopbits are : 1
escape is : C-a
local echo is : no
noinit is : no
noreset is : yes
hangup is : no
nolock is : yes
send_cmd is : sz -vv
receive_cmd is : rz -vv -E
imap is :
omap is :
emap is : crcrlf,delbs,
logfile is : none
initstring : none
exit_after is : not set
exit is : no
Type [C-a] [C-h] to see available commands
Terminal ready
Sciserver Testapp Built On: Mar 19 2025 10:50:19
Sciserver Version: 11.0.0-REL.MCUSDK.11.00.00.05+
RM_PM_HAL Version: v11.00.09
Starting Sciserver..... PASSED
[IPC RPMSG ECHO] Version: REL.MCUSDK.09.00.00.16 (Mar 19 2025 10:50:35):
Sciserver Testapp Built On: Mar 19 2025 10:50:19
Sciserver Version: 11.0.0-REL.MCUSDK.11.00.00.05+
RM_PM_HAL Version: v11.00.09
Starting Sciserver..... PASSED
[IPC RPMSG ECHO] Version: REL.MCUSDK.09.00.00.16 (Mar 19 2025 10:50:35):
Sciserver Testapp Built On: Mar 19 2025 10:50:19
Sciserver Version: 11.0.0-REL.MCUSDK.11.00.00.05+
RM_PM_HAL Version: v11.00.09
Starting Sciserver..... PASSED
[IPC RPMSG ECHO] Version: REL.MCUSDK.09.00.00.16 (Mar 19 2025 10:50:35):
Sciserver Testapp Built On: Mar 19 2025 10:50:19
Sciserver Version: 11.0.0-REL.MCUSDK.11.00.00.05+
RM_PM_HAL Version: v11.00.09
Starting Sciserver..... PASSED
[IPC RPMSG ECHO] Version: REL.MCUSDK.09.00.00.16 (Mar 19 2025 10:50:35):
Sciserver Testapp Built On: Mar 19 2025 10:50:19
Sciserver Version: 11.0.0-REL.MCUSDK.11.00.00.05+
RM_PM_HAL Version: v11.00.09
Starting Sciserver..... PASSED
[IPC RPMSG ECHO] Version: REL.MCUSDK.09.00.00.16 (Mar 19 2025 10:50:35):
Sciserver Testapp Built On: Mar 19 2025 10:50:19
Sciserver Version: 11.0.0-REL.MCUSDK.11.00.00.05+
RM_PM_HAL Version: v11.00.09
Starting Sciserver..... PASSED
[IPC RPMSG ECHO] Version: REL.MCUSDK.09.00.00.16 (Mar 19 2025 10:50:35):
Sciserver Testapp Built On: Mar 19 2025 10:50:19
Sciserver Version: 11.0.0-REL.MCUSDK.11.00.00.05+
RM_PM_HAL Version: v11.00.09
Starting Sciserver..... PASSED