This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: AM623: EMMC configuration for the main board

Part Number: AM623


Tool/software:

My circuit design uses the AM6234 as the main IC, paired with a THGAMVG7T13BAI eMMC card. However, due to my company's requirement for a second-source solution, I identified the SDINBDA6-16G as an alternative.

I tested the SDINBDA6-16G by replacing the THGAMVG7T13BAI on a previously functioning circuit board, but I'm currently experiencing issues getting it to operate correctly. I’d appreciate any feedback or suggestions you might have.

cmd

EEPROM cust_eth_mac=00:e0:db:8e:b9:46
Hit any key to stop autoboot: 0
=> mmc partconf 0 1 1 1
=> mmc bootbus 0 2 0 0
Set to BOOT_BUS_WIDTH = 0x2, RESET = 0x0, BOOT_MODE = 0x0
=> mmc rst-function 0 1
=> setenv mmcdev 0
=> setenv bootpart 0:6
=> setenv rauc_launch ""
=> saveenv
Saving Environment to MMC... Writing to redundant MMC(0)... MMC: block number 0x3100 exceeds max(0x2000)
failed
failed