This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: Use wdr mode to create binfile ,camera no im

Part Number: AM62A7


Tool/software:

Hi TI Experts

I set WDR_MODE 1 in imx219_properties.txt to generated XML, and then generated three bin file.

When I applied they to the development board, the camera screen was completely black.

I checked the exposure and gain register data and found that they were normal. The screen should be displayed.

Here is my imx219_properties.txt:

Do I need to change another params ?

SENSOR_ID 219
PRJ_DIR ../imx219_output
SENSOR_NAME imx219
SENSOR_DCC_NAME IMX219

SENSOR_WIDTH 1920
SENSOR_HEIGHT 1280

# 0=RGGB; 1=GRBG; 2=GBRG; 3=BGGR, 4=MONO
COLOR_PATTERN 3

# sensor mode: 0 for linear (no decompanding), 1 for WDR (decompanding)
WDR_MODE 0

# raw sensor image BIT_DEPTH: it may be 8, 10, or 12 for linear sensors; typically 12 for WDR mode because of companding
BIT_DEPTH 12

# WDR BIT_DEPTH: WDR raw sensor image bitdepth after decompanding, typically 20 or 24
WDR_BIT_DEPTH 24

# WDR decompanding knee points (comma separated without spaces in between)
WDR_KNEE_X 0,512,1408,2176,4095,65535
WDR_KNEE_Y 0,2048,16384,65536,1048063,1048063

# Sensor black level to subtract before decompanding (for linear sensors only and some Sony WDR sensors)
BLACK_PRE  64

# Sensor black level to subtract after decompanding (for most WDR sensors and all linear sensors)
BLACK_POST  0

# GAMMA value for compressing 20/24-bit WDR raw to 16-bit ISP internal
# typically around 50 (0.5) for 24-bit WDR sensors and 70 (0.7) for 20-bit sensors
GAMMA_PRE 50

# LSB location for H3A input bit range (from bit-H3A_INPUT_LSB to bit-H3A_INPUT_LSB+9) 
H3A_INPUT_LSB 0

# Choose the default gamma curve used for YUV output: 0 for BT709, 1 for a high contrast gamma curve
YUV_GAMMA 1

Best Regards

Meng