Other Parts Discussed in Thread: AM6442
Tool/software:
Hi,
I am new to the AM64x software development and had the following basic questions:
1. I know AM64x includes different processor cores: A53 cores are suitable for computation and typically run in Linux; R5F cores are for control and run in RTOS or no RTOS. However, it is a bit unclear to envision the potential applications I can utilize all these processor cores. Take AM64x EVM (AM6442) as the example, can I get some examples of what applications can be implemented in A53, then passing data from A53 to R5F cores, then maybe passing the results back to A53?
2. AM64x EVM has 4 R5F cores, what are the default MCU applications run on these cores?
3. Does one of the R5F cores implement CPSW based ethernet firmware? For example, if I ran TSN PTP application in Linux, are the TSN PTP, frame preemption, EST features done in one of the R5F cores?
Thank you!