Hello,
I am seeking assistance with a question I received below:
"We want to insure that the AM3517 can directly drive a large format LCD display without the need of converting from 24-bit parallel data to HDMI or DVI and then back to parallel data at the display. The AM3517 processor and its circuit card will be positioned behind the LCD display in this design allowing us to directly connect to the display and therefore minimize or eliminate cost associated with converting the display signals to HDMI or DVI. Is there someone on your team that can help with setting up the display registers in the AM3517 or at least confirm that a certain LCD display (to be picked soon) can be interfaced properly to the AM3517’s display sub-system? We don’t want to get so far down a design path and find out that it can’t be done".
Thanks,
Todd