In the case of multiple hardware platforms across a vast product line (using DM368, DM365, DM6467, DM355, etc...) is there any way for the code to determine which processor it is running on? As in some type of processor ID register with information as to the target hardware device?