This is a companion FAQ for
[FAQ] [Alert] DM R5F can crash in certain conditions: AM62x, AM62Ax, AM62Dx, AM62Px, AM67, AM67A
Please read the alert first. You can also find more information in the main FAQ here:
[FAQ] DM R5F can crash in certain conditions: AM62x, AM62Ax, AM62Dx, AM62Px, AM67, AM67A
This FAQ applies to AM62x, AM62Ax, AM62Dx, AM62Px.
The DM R5F does not need to be running the ipc_rpmsg_echo_linux project, as discussed in [FAQ] Does the DM R5F need to run the IPC Echo demo task? .
We can use the empty project if we want to remove all other code from the DM R5F core, other than the critical device manager (DM) task. However, there are multiple things that we need to keep in mind if we want to use the empty project.