Other Parts Discussed in Thread: TVP7002
HI , TI engineer
I want to use TMDXEVM8168 to compress two chanle 1080P60 in H264 and save them into file.
I want to use two instance of h264venc , two instance of vfcc , and two instance of dei ,but when I
convert h264venc to IDLE state,it is block.
The version of sdk I used is 5_01_01_80,is two 1080p60 compressed supported in this version or any other problem?
Thank you.