This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: apps_python framerate question

Part Number: SK-AM62A-LP


Tool/software:

Dear Expert,

I am using IMX219, IMX335 and a fingers 1080p Hi-Res USB camera with apps_python. Can you please mention the maximum frame per second compatibility of apps_python. Is there any limiters in fps.

I checked framerate in input and output section of app_config.yaml is set between the values 15 to 30 but it seems 20 frames or something in every video. Sometimes app crashes when running.
Gone through the documentation of IMX219. There seems 30 fps @ 1920x1080.

Warm Regards,
Sajan

  • Hi Sajan,

    The assigned topic expert is currently out of office and will return on September 2nd. Please expect a delay in response. Thank you for your patience.

    Regards,
    Johnson

  • Hi Sajan,

    Using apps_python on the AM62A should imply that you are running analytics on the board. In that case, the inference would limit the framerate of the output. In case of the app crashing, could you share the yaml config?

    Best Regards,
    Jay

  • Hello Jay,

    could you share the yaml config

    title: "Preview"
    inputs:
        input0:
            source: /dev/video-imx219-cam0
            subdev-id: /dev/v4l-imx219-subdev0
            format: rggb
            width: 1920
            height: 1080
            framerate: 15
    models:
        model0:
            model_path: /opt/model_zoo/samplemodel
            topN: 1
    outputs:
        output0:
            sink: kmssink
            width: 1920
            height: 1080
    flows:
        flow0: [input0,model0,output0]

    would limit the framerate of the output

    But In my finding, seems no change affects when I modify the input and output frame rate. It will record the video in 20fps.

    Warm Regards,
    Sajan

  • Hi Sajan,

    It seems that the issue is with the pipeline that apps_python constructs. The gstreamer nodes used in those don't respect the framerate and send data at the maximum possible framerate. If limiting the framerate is important, a videorate element can be added. This will create the issue of duplication of frames if the framerate dips. For example, if you have set the framerate to 30 and it dips to 26, videorate will force the pipeline to 30fps by duplicating some frames.

    If this satisfies your requirements, here is the corresponding patch (SDK 11.01):

    --- gst_wrapper.py
    +++ gst_wrapper.py
    @@ -1198,6 +1198,8 @@
    
         element = make_element("appsrc", property=property)
         post_proc_elements += element
    +    element = make_element("videorate", property={"max-rate": int(eval(flow.input.fps))})
    +    post_proc_elements += element
    
         caps = "video/x-raw, format=NV12, width=%d, height=%d" % (
             flow.sensor_width,
    

    Nevertheless, I have raised a bug report and will keep an eye on its progress.

    Best Regards,
    Jay

  • Hello Jay,

    I tried updating the gst_wrapper.py with the patch you gave. But It doesn't works for me. When the app starts green screen cames and seems the below error.

    libtidl_onnxrt_EP loaded 0x43b6680 
    Final number of subgraphs created are : 1, - Offloaded Nodes - 124, Total Nodes - 124 
    APP: Init ... !!!
       697.510398 s: MEM: Init ... !!!
       697.510479 s: MEM: Initialized DMA HEAP (fd=5) !!!
       697.510672 s: MEM: Init ... Done !!!
       697.510704 s: IPC: Init ... !!!
       697.528775 s: IPC: Init ... Done !!!
    REMOTE_SERVICE: Init ... !!!
    REMOTE_SERVICE: Init ... Done !!!
       697.533507 s: GTC Frequency = 200 MHz
    APP: Init ... Done !!!
       697.533663 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_ERROR
       697.533679 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_WARNING
       697.533690 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_INFO
       697.535168 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-0 
       697.535467 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-1 
       697.535760 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-2 
       697.536063 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-3 
       697.536100 s:  VX_ZONE_INFO: [tivxInitLocal:126] Initialization Done !!!
       697.536131 s:  VX_ZONE_INFO: Globally Disabled VX_ZONE_INFO
    ==========[INPUT PIPELINE(S)]==========
    
    [PIPE-0]
    
    v4l2src device=/dev/video-imx219-cam0 io-mode=5 pixel-aspect-ratio=None ! queue leaky=2 ! capsfilter caps="video/x-bayer, width=(int)1920, height=(int)1080, format=(string)rggb;" ! tiovxisp dcc-isp1
    split_01. ! queue ! capsfilter caps="video/x-raw, width=(int)1920, height=(int)1080;" ! tiovxdlcolorconvert out-pool-size=4 ! capsfilter caps="video/x-raw, format=(string)RGB;" ! appsink max-buffer0
    split_01. ! queue ! capsfilter caps="video/x-raw, width=(int)1188, height=(int)668;" ! tiovxmultiscaler target=1 ! capsfilter caps="video/x-raw, width=(int)454, height=(int)256;" ! tiovxdlcolorconv0
    
    
    ==========[OUTPUT PIPELINE]==========
    
    appsrc do-timestamp=True format=3 block=True name=post_0 ! videorate max-rate=20 ! tiovxdlcolorconvert ! capsfilter caps="video/x-raw, format=(string)NV12, width=(int)1920, height=(int)1080;" ! kms6
    
    ^C[ERROR] GStreamer error: negotiation problem.
    APP: Deinit ... !!!
    REMOTE_SERVICE: Deinit ... !!!
    REMOTE_SERVICE: Deinit ... Done !!!
    


    Warm Regards,
    Sajan

  • Hi Sajan,

    It seems that you need to set the appsrc property 'is-live' to true. I seem to have missed the same in the patch. Apologies for the same. Here is the updated patch:

    --- gst_wrapper.py
    +++ gst_wrapper.py
    @@ -1188,6 +1188,7 @@
             "block": True,
             "do-timestamp": True,
             "name": flow.gst_post_sink_name,
    +        "is-live": True,
         }
    
         for o in flow.outputs:
    @@ -1197,6 +1198,8 @@
                 break
    
         element = make_element("appsrc", property=property)
    +    post_proc_elements += element
    +    element = make_element("videorate", property={"max-rate": int(eval(flow.input.fps))})
         post_proc_elements += element
    
         caps = "video/x-raw, format=NV12, width=%d, height=%d" % (

    If the issue still persists, please share your SDK version as well.

    For reference, here is some info on live sources from gstreamer wiki: https://gstreamer.freedesktop.org/documentation/additional/design/live-source.html?gi-language=c.

    Best Regards,
    Jay

  • Hi Jay,

    It is now working but seems framerate issue. When I make the input and output frame rate to 30, the frame rate becomes 3 to 5 fps. I got the almost correct frame rate at 20 and 24 fps.

    Warm Regards,
    Sajan

  • Hi Sajan,

    I do see this issue. As a workaround, you can set a mosaic at 0,0 with 1920x1080 dimensions. This seems to make the latency better. The resulting flow(in yaml config) should look like this:

    flow0: [input0, model0, output0, [0, 0, 1920, 1080]]

    On my end, with this, I get around 22fps when framerate is set to 30 in test config. I would still suggest going with the base SDK code for getting the maximum performance because videorate does seem to have performance implications in general.

    In the meantime, I will try to figure out where this issue actually comes from and figure out a more complete fix.

    Best Regards,
    Jay