Hi,
Under the Run Instructions for Codec Engine Examples , I can run codec engine examples on the DM8168 EVM. But
can they be run on CCSv5 with simulator? Thanks a lot!
sunzhao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Zhao,
It depends on the simulator. If you have a simulator for only the DSP, then you can only run a local Codec Example. If you have a system simulator, where the entire device is simulated, and you have a Linux BSP which supports the simulator, then you could boot Linux on the host and run a remote Codec Example. Typically, this is hard to setup and the EVM is easier to use.
~ Ramsey