Part Number: AM62P
Tool/software:
Hi
I was working on the example am62p evm enable lvds panel (ti-sk-lcd1) same as example.
sdk version is 11.01.05.03
using
tisdk-default-image-am62pxx-evm.wic.xz
And i tried two methods to enable the LVDS panel.
Base on the am62p user guide as below:
In this method, i setting an overlay as 10 used as "Microtips Technology USA 10.1” WUXGA (1920x1200) OLDI panel" but seems like setting env under Uboot doesn't work.
And secound, i try the method 2 as am62 user guide
i rebuild dts to generate k3-am62p5-sk-microtips-mf101hie-panel.dtbo
And push in the device and set the nEnv.txt
name_overlays=ti/k3-am62p5-sk-microtips-mf101hie-panel.dtbo
terminate called after throwing an instance of '[ 82.773575] kauditd_printk_skb: 1 callbacks suppressed
std::runtime_error'
what(): failed to find DRM cards
[ 82.773595] audit: type=1701 audit(1651171636.080:29): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=1250 comm="kmsprint" exe="/usr/bin/kmsprint" sig=6 res=1
[ 82.807386] audit: type=1334 audit(1651171636.116:30): prog-id=17 op=LOAD
[ 82.814356] audit: type=1334 audit(1651171636.124:31): prog-id=18 op=LOAD
Aborted (core dumped)
root@am62pxx-evm:~# [ 83.410156] audit: type=1334 audit(1651171636.720:32): prog-id=18 op=UNLOAD
[ 83.417311] audit: type=1334 audit(1651171636.720:33): prog-id=17 op=UNLOAD
[ 2.666718] vmap allocation for size 483328 failed: use vmalloc=<size> to increase size
[ 2.683248] systemd: vmalloc error: size 479232, vm_struct allocation failed, mode:0xcc0(GFP_KERNEL), nodemask=(null),cpuset=/,mems_allowed=0
[ 2.783567] __vmalloc_node_range+0x590/0x740
[ 5.122889] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
[ 5.259554] vmap allocation for size 32768 failed: use vmalloc=<size> to increase size
[ 5.307101] vmap allocation for size 135168 failed: use vmalloc=<size> to increase size
[ 5.424905] vmap allocation for size 483328 failed: use vmalloc=<size> to increase size
[ 5.446547] vmap allocation for size 483328 failed: use vmalloc=<size> to increase size
[ 5.479668] vmap allocation for size 483328 failed: use vmalloc=<size> to increase size
[ 5.532251] vmap allocation for size 57344 failed: use vmalloc=<size> to increase size
[ 7.060714] vmap allocation for size 24576 failed: use vmalloc=<size> to increase size
[ 7.075133] vmap allocation for size 24576 failed: use vmalloc=<size> to increase size
[ 10.381227] vmap allocation for size 126976 failed: use vmalloc=<size> to increase size
[ 10.422959] vmap allocation for size 483328 failed: use vmalloc=<size> to increase size
[ 10.467649] vmap allocation for size 483328 failed: use vmalloc=<size> to increase size
[ 10.497398] vmap allocation for size 483328 failed: use vmalloc=<size> to increase size
[ 10.602533] vmap allocation for size 483328 failed: use vmalloc=<size> to increase size
[ 10.627038] vmap allocation for size 483328 failed: use vmalloc=<size> to increase size