Part Number: AM625
Tool/software:
Hi Expert,
customer is using sdk11.1 and using the dummy key HSSE board, they follow the guide to boot form emmc, but it reports error as below, pls help see what is the issue?
U-Boot SPL 2023.04-00001-gf5b119738d-dirty (Aug 30 2025 - 13:24:45 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
SPL initial stack usage: 13376 bytes
Trying to boot from MMC1
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Starting ATF on ARM64 core...
NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE: BL31: Built : 00:42:57, Jan 13 2023
U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
SPL initial stack usage: 1856 bytes
MMC: no card present
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:1
Error: could not access storage.
Trying to boot from MMC1
Authentication passed
Authentication passed
U-Boot 2023.04-00001-gf5b119738d-dirty (Aug 30 2025 - 13:25:24 +0800)
SoC: AM62X SR1.0 HS-SE
Model: Texas Instruments AM625 SK
EEPROM not available at 80, trying to read at 81
Board: AM62B-SKEVM-P1 rev A
DRAM: 2 GiB
Core: 71 devices, 31 uclasses, devicetree: separate
MMC: mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from MMC... OK
In: serial
Out: serial
Err: serial
Unidentified board claims AM62B-SKEVM-P1 in eeprom header
Net: eth0: ethernet@8000000port@1
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0(part 0) is current device
SD/MMC found on device 0
Failed to load 'boot.scr'
Can't set block device
## Error: "main_cpsw0_qsgmii_phyinit" not defined
8686034 bytes read in 64 ms (129.4 MiB/s)
name_fit_config=conf-ti_k3-am625-sk.dtb
## Loading kernel from FIT Image at 90000000 ...
Using 'conf-ti_k3-am625-sk.dtb' configuration
Verifying Hash Integrity ... fit_config_verify_required_keys: No signature node found: FDT_ERR_NOTFOUND
Bad Data Hash
ERROR: can't get kernel image!
switch to partitions #0, OK
mmc0(part 0) is current device
Scanning mmc 0:1...
MMC: no card present
No EFI system partition
No EFI system partition
Failed to persist EFI variables
BootOrder not defined
EFI boot manager: Cannot load any image
MMC: no card present
starting USB...
Bus usb@31100000: generic_phy_get_bulk : no phys property
Register 1000840 NbrPorts 1
Starting the controller
USB XHCI 1.10
scanning bus usb@31100000 for devices... 1 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found
Device 0: unknown device
ethernet@8000000port@1 Waiting for PHY auto negotiation to complete......... TIMEOUT !
am65_cpsw_nuss_port ethernet@8000000port@1: phy_startup failed
am65_cpsw_nuss_port ethernet@8000000port@1: am65_cpsw_start end error
missing environment variable: pxeuuid
Retrieving file: pxelinux.cfg/01-1c-63-49-22-4f-8a
ethernet@8000000port@1 Waiting for PHY auto negotiation to complete......... TIMEOUT !
am65_cpsw_nuss_port ethernet@8000000port@1: phy_startup failed
am65_cpsw_nuss_port ethernet@8000000port@1: am65_cpsw_start end error
Retrieving file: pxelinux.cfg/00000000
BR,
Biao