This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Nand flash - Reading error

Other Parts Discussed in Thread: DM3730, ADS7846, AM3703

Hi all,

I have flashed all the prebuilt images ,

x-load.bin.ift, u-boot.bin, uImage and ubi.img.

While booting , it is strucking after the uImage uncompressing,

what might be the problem ?

 

Regards,

santosh vastrad

  • The information is very limited, in order to understand the issue better can you provide information -

     - Which board or EVM are you using? Is it your own custom board?

     - Which kernel version are you using?

     - Which Kernel Sources?

     

    Also, you may want to enable EARLY_PRINTK config option which may give you some pointers on whats going on after uncompressing kernel.

     

    Thanks,

    Vaibhav

  • Hi vaibhav thanks for the reply,

    �����������������������������������������������������������������������������������������������������������������������������������������������������������������������0
    buad_divisor   = 1a
    size[0] = 0
    size[1] = 0
    size[2] = 2
    size[3] = 1a
    size[4] = 0
    size[5] = 83
    size[6] = 3
    size[7] = c1
    size[8] = 0
    size[9] = 0
    NS16550_init


    U-Boot 2010.06-rc1 (Oct 18 2011 - 10:18:51)

    OMAP34xx/35xx-GP ES2.1, CPU-OPP2 L3-165MHz
    OMAP3 Beagle board + LPDDR/NAND
    I2C:   ready
    DRAM:  256 MiB
    NAND:  Hello hi
    Check for 16 bit
    512 MiB
    In:    serial
    Out:   serial
    Err:   serial
    Beagle Rev Ax/Bx
    Die ID #63b800029e380000016830c501033011
    Hit any key to stop autoboot:  0
    setenv bootargs console=ttyS2,115200n8 ubi.mtd=4 root=ubi0:rootfs rootfstype=ubifs rw rootwait nohz=off init=/sbin/<INTERRUPT>.console=ttyS2ndroidboot.console=ttyS2
    OMAP3 beagleboard.org # setenv bootargs console=ttyS2,115200n8 ubi.mtd=4 root=ubi0:rootfs rootfstype=ubifs rw rootwait nohz=off init=/sbin/init androidboot.console=tty2
    Unknown command 'setenv' - try 'help'
    OMAP3 beagleboard.org # setenv bootargs console=ttyS2,115200n8 ubi.mtd=4 root=ubi0:rootfs rootfstype=ubifs rw rootwait nohz=off init=/sbin/init
    OMAP3 beagleboard.org # saveenv
    Saving Environment to NAND...
    Erasing Nand...
    Erasing at 0x260000 -- 100% complete.
    Writing to Nand... done
    OMAP3 beagleboard.org # boot

    NAND read: device 0 offset 0x280000, size 0x400000
     4194304 bytes read: OK
    ## Booting kernel from Legacy Image at 80000000 ...
       Image Name:   Linux-2.6.32
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    3312156 Bytes = 3.2 MiB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux.....................................................................................................................................................
    [    0.000000] Linux version 2.6.32 (venkatraju@localhost.localdomain) (gcc version 4.2.0 20070413 (prerelease) (CodeSourcery Sourcery G++ Lite 2007q1-10)) #45 PREEMPT1
    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
    [    0.000000] CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
    [    0.000000] Machine: OMAP3 Beagle Board
    [    0.000000] Memory policy: ECC disabled, Data cache writeback
    [    0.000000] OMAP3630/DM3730 ES1.0 (l2cache iva neon isp 192mhz_clk )
    [    0.000000] SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x100000
    [    0.000000] Reserving 4194304 bytes SDRAM for VRAM
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024
    [    0.000000] Kernel command line: console=ttyS2,115200n8 ubi.mtd=4 root=ubi0:rootfs rootfstype=ubifs rw rootwait nohz=off init=/sbin/init
    [    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
    [    0.000000] Memory: 256MB = 256MB total
    [    0.000000] Memory: 247936KB available (6072K code, 1066K data, 304K init, 0K highmem)
    [    0.000000] Hierarchical RCU implementation.
    [    0.000000] NR_IRQS:402
    [    0.000000] Clocking rate (Crystal/Core/MPU): 26.0/332/600 MHz
    [    0.000000] Reprogramming SDRC clock to 332000000 Hz
    [    0.000000] GPMC revision 5.0
    [    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts
    [    0.000000] Total of 96 interrupts on 1 active controller
    [    0.000000] OMAP GPIO hardware version 2.5
    [    0.000000] OMAP clockevent source: GPTIMER12 at 32768 Hz
    [    0.000000] Console: colour dummy device 80x30
    [    0.000000] Calibrating delay loop... 505.22 BogoMIPS (lpj=1974272)
    [    0.000000] Mount-cache hash table entries: 512
    [    0.000000] CPU: Testing write buffer coherency: ok
    [    0.000000] tmpfs: No value for mount option 'mode'
    [    0.000000] devtmpfs: initialized
    [    0.000000] regulator: core version 0.5
    [    0.000000] NET: Registered protocol family 16
    [    0.000000] kobject (c067bb00): tried to init an initialized object, something is seriously wrong.
    [    0.000000] [<c0059d60>] (unwind_backtrace+0x0/0xdc) from [<c02500c8>] (kobject_init+0x3c/0x7c)
    [    0.000000] [<c02500c8>] (kobject_init+0x3c/0x7c) from [<c02aeacc>] (device_initialize+0x24/0x8c)
    [    0.000000] [<c02aeacc>] (device_initialize+0x24/0x8c) from [<c02b30a8>] (platform_device_register+0x10/0x1c)
    [    0.000000] [<c02b30a8>] (platform_device_register+0x10/0x1c) from [<c0010c68>] (omap_register_i2c_bus+0x60/0x70)
    [    0.000000] [<c0010c68>] (omap_register_i2c_bus+0x60/0x70) from [<c0010e6c>] (omap3_beagle_init+0xa8/0x3ec)
    [    0.000000] [<c0010e6c>] (omap3_beagle_init+0xa8/0x3ec) from [<c000b9e8>] (customize_machine+0x1c/0x2c)
    [    0.000000] [<c000b9e8>] (customize_machine+0x1c/0x2c) from [<c005436c>] (do_one_initcall+0x54/0x198)
    [    0.000000] [<c005436c>] (do_one_initcall+0x54/0x198) from [<c00088a8>] (kernel_init+0x9c/0x118)
    [    0.000000] [<c00088a8>] (kernel_init+0x9c/0x118) from [<c0055910>] (kernel_thread_exit+0x0/0x8)
    [    0.000000] ------------[ cut here ]------------
    [    0.000000] WARNING: at fs/sysfs/dir.c:477 sysfs_add_one+0x108/0x134()
    [    0.000000] sysfs: cannot create duplicate filename '/devices/platform/i2c_omap.2'
    [    0.000000] Modules linked in:
    [    0.000000] [<c0059d60>] (unwind_backtrace+0x0/0xdc) from [<c00824bc>] (warn_slowpath_common+0x4c/0x68)
    [    0.000000] [<c00824bc>] (warn_slowpath_common+0x4c/0x68) from [<c0082514>] (warn_slowpath_fmt+0x28/0x38)
    [    0.000000] [<c0082514>] (warn_slowpath_fmt+0x28/0x38) from [<c014dea4>] (sysfs_add_one+0x108/0x134)
    [    0.000000] [<c014dea4>] (sysfs_add_one+0x108/0x134) from [<c014e470>] (create_dir+0x4c/0x98)
    [    0.000000] [<c014e470>] (create_dir+0x4c/0x98) from [<c014e4f8>] (sysfs_create_dir+0x3c/0x54)
    [    0.000000] [<c014e4f8>] (sysfs_create_dir+0x3c/0x54) from [<c025046c>] (kobject_add_internal+0xe0/0x1bc)
    [    0.000000] [<c025046c>] (kobject_add_internal+0xe0/0x1bc) from [<c02509ec>] (kobject_add+0x50/0x64)
    [    0.000000] [<c02509ec>] (kobject_add+0x50/0x64) from [<c02aee94>] (device_add+0x94/0x494)
    [    0.000000] [<c02aee94>] (device_add+0x94/0x494) from [<c02b303c>] (platform_device_add+0xf8/0x154)
    [    0.000000] [<c02b303c>] (platform_device_add+0xf8/0x154) from [<c0010c68>] (omap_register_i2c_bus+0x60/0x70)
    [    0.000000] [<c0010c68>] (omap_register_i2c_bus+0x60/0x70) from [<c0010e6c>] (omap3_beagle_init+0xa8/0x3ec)
    [    0.000000] [<c0010e6c>] (omap3_beagle_init+0xa8/0x3ec) from [<c000b9e8>] (customize_machine+0x1c/0x2c)
    [    0.000000] [<c000b9e8>] (customize_machine+0x1c/0x2c) from [<c005436c>] (do_one_initcall+0x54/0x198)
    [    0.000000] [<c005436c>] (do_one_initcall+0x54/0x198) from [<c00088a8>] (kernel_init+0x9c/0x118)
    [    0.000000] [<c00088a8>] (kernel_init+0x9c/0x118) from [<c0055910>] (kernel_thread_exit+0x0/0x8)
    [    0.000000] ---[ end trace 1b75b31a2719ed1c ]---
    [    0.000000] kobject_add_internal failed for i2c_omap.2 with -EEXIST, don't try to register things with the same name in the same directory.
    [    0.000000] [<c0059d60>] (unwind_backtrace+0x0/0xdc) from [<c02504e8>] (kobject_add_internal+0x15c/0x1bc)
    [    0.000000] [<c02504e8>] (kobject_add_internal+0x15c/0x1bc) from [<c02509ec>] (kobject_add+0x50/0x64)
    [    0.000000] [<c02509ec>] (kobject_add+0x50/0x64) from [<c02aee94>] (device_add+0x94/0x494)
    [    0.000000] [<c02aee94>] (device_add+0x94/0x494) from [<c02b303c>] (platform_device_add+0xf8/0x154)
    [    0.000000] [<c02b303c>] (platform_device_add+0xf8/0x154) from [<c0010c68>] (omap_register_i2c_bus+0x60/0x70)
    [    0.000000] [<c0010c68>] (omap_register_i2c_bus+0x60/0x70) from [<c0010e6c>] (omap3_beagle_init+0xa8/0x3ec)
    [    0.000000] [<c0010e6c>] (omap3_beagle_init+0xa8/0x3ec) from [<c000b9e8>] (customize_machine+0x1c/0x2c)
    [    0.000000] [<c000b9e8>] (customize_machine+0x1c/0x2c) from [<c005436c>] (do_one_initcall+0x54/0x198)
    [    0.000000] [<c005436c>] (do_one_initcall+0x54/0x198) from [<c00088a8>] (kernel_init+0x9c/0x118)
    [    0.000000] [<c00088a8>] (kernel_init+0x9c/0x118) from [<c0055910>] (kernel_thread_exit+0x0/0x8)
    [    0.000000] Found NAND on CS0
    [    0.000000] Registering NAND on CS0
    [    0.000000] Unable to get DVI reset GPIO
    [   85.731109] OMAP DMA hardware revision 5.0
    [   85.764160] bio: create slab <bio-0> at 0
    [   85.767181] SCSI subsystem initialized
    [   85.771331] usbcore: registered new interface driver usbfs
    [   85.771820] usbcore: registered new interface driver hub
    [   85.772125] usbcore: registered new device driver usb
    [   85.772979] i2c_omap i2c_omap.1: bus 1 rev4.0 at 2600 kHz
    [   85.776580] twl4030: PIH (irq 7) chaining IRQs 368..375
    [   85.776611] twl4030: power (irq 373) chaining IRQs 376..383
    [   85.777099] twl4030: gpio (irq 368) chaining IRQs 384..401
    [   85.780059] regulator: VUSB1V5: 1500 mV normal standby
    [   85.780639] regulator: VUSB1V8: 1800 mV normal standby
    [   85.781219] regulator: VUSB3V1: 3100 mV normal standby
    [   85.782684] twl4030_usb twl4030_usb: Initialized TWL4030 USB module
    [   85.784393] regulator: VMMC1: 1850 <--> 3150 mV normal standby
    [   85.784973] regulator: VDAC: 1800 mV normal standby
    [   85.785583] regulator: VPLL2: 1800 mV normal standby
    [   85.786163] regulator: VSIM: 1800 <--> 3000 mV normal standby
    [   85.786804] regulator: VAUX3: 1800 mV normal standby
    [   85.787506] regulator: VAUX4: 1800 mV normal standby
    [   85.787689] i2c_omap i2c_omap.3: bus 3 rev4.0 at 100 kHz
    [   85.791412] cfg80211: Using static regulatory domain info
    [   85.791442] cfg80211: Regulatory domain: 00
    [   85.791442]     (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp)
    [   85.791473]     (2402000 KHz - 2472000 KHz @ 40000 KHz), (600 mBi, 2000 mBm)
    [   85.791473]     (2457000 KHz - 2482000 KHz @ 20000 KHz), (600 mBi, 2000 mBm)
    [   85.791503]     (2474000 KHz - 2494000 KHz @ 20000 KHz), (600 mBi, 2000 mBm)
    [   85.791534]     (5170000 KHz - 5250000 KHz @ 40000 KHz), (600 mBi, 2000 mBm)
    [   85.791534]     (5735000 KHz - 5835000 KHz @ 40000 KHz), (600 mBi, 2000 mBm)
    [   85.791595] cfg80211: Calling CRDA to update world regulatory domain
    [   85.791961] Switching to clocksource 32k_counter
    [   85.803558] musb_hdrc: version 6.0, musb-dma, otg (peripheral+host), debug=0
    [   85.806030] musb_hdrc: USB OTG mode controller at fa0ab000 using DMA, IRQ 92
    [   85.807098] NET: Registered protocol family 2
    [   85.807281] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
    [   85.807952] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
    [   85.808166] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
    [   85.808258] TCP: Hash tables configured (established 8192 bind 8192)
    [   85.808288] TCP reno registered
    [   85.808288] UDP hash table entries: 256 (order: 0, 4096 bytes)
    [   85.808319] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    [   85.808532] NET: Registered protocol family 1
    [   85.809020] RPC: Registered udp transport module.
    [   85.809020] RPC: Registered tcp transport module.
    [   85.809051] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [   85.818725] VFS: Disk quotas dquot_6.5.2
    [   85.818847] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    [   85.820587] JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
    [   85.821228] msgmni has been set to 484
    [   85.824798] alg: No test for stdrng (krng)
    [   85.825347] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 253)
    [   85.825347] io scheduler noop registered
    [   85.825378] io scheduler deadline registered
    [   85.825531] io scheduler cfq registered (default)
    [   85.885894] OMAP DSS rev 2.0
    [   85.885955] OMAP DISPC rev 3.0
    [   85.886016] OMAP VENC rev 2
    [   85.886413] OMAP DSI rev 1.0
    [   86.213989] embest_panel_probe was invoked, Baby.
    [   86.214019] embest_panel_probe was invoked, Baby.
    [   86.236724] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    [   86.256317] serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654
    [   86.274353] serial8250.1: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654
    [   86.292236] serial8250.2: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654
    [   87.200683] console [ttyS2] enabled
    [   87.217254] brd: module loaded
    [   87.226989] loop: module loaded
    [   87.232299] omap2-nand driver initializing
    [   87.236694] NAND device: Manufacturer ID: 0xad, Chip ID: 0xbc (Hynix NAND 512MiB 1,8V 16-bit)
    [   87.245788] cmdlinepart partition parsing not available
    [   87.251037] Creating 5 MTD partitions on "omap2-nand":
    [   87.256317] 0x000000000000-0x000000080000 : "X-Loader"
    [   87.263397] 0x000000080000-0x000000260000 : "U-Boot"
    [   87.270477] 0x000000260000-0x000000280000 : "U-Boot Env"
    [   87.277252] 0x000000280000-0x000000680000 : "Kernel"
    [   87.285034] 0x000000680000-0x000020000000 : "File System"
    [   87.472625] UBI: attaching mtd4 to ubi0
    [   87.476501] UBI: physical eraseblock size:   131072 bytes (128 KiB)
    [   87.482910] UBI: logical eraseblock size:    129024 bytes
    [   87.488342] UBI: smallest flash I/O unit:    2048
    [   87.493072] UBI: sub-page size:              512
    [   87.497772] UBI: VID header offset:          512 (aligned 512)
    [   87.503662] UBI: data offset:                2048
    [   88.395843] UBI: attached mtd4 to ubi0
    [   88.399658] UBI: MTD device name:            "File System"
    [   88.405273] UBI: MTD device size:            505 MiB
    [   88.410308] UBI: number of good PEBs:        4044
    [   88.415069] UBI: number of bad PEBs:         0
    [   88.419555] UBI: max. allowed volumes:       128
    [   88.424194] UBI: wear-leveling threshold:    4096
    [   88.428955] UBI: number of internal volumes: 1
    [   88.433441] UBI: number of user volumes:     1
    [   88.437927] UBI: available PEBs:             0
    [   88.442413] UBI: total number of reserved PEBs: 4044
    [   88.447387] UBI: number of PEBs reserved for bad PEB handling: 40
    [   88.453552] UBI: max/mean erase counter: 1/0
    [   88.457855] UBI: image sequence number: 0
    [   88.462097] UBI: background thread "ubi_bgt0d" started, PID 504
    [   88.476715] Fixed MDIO Bus: probed
    [   88.481262] PPP generic driver version 2.4.2
    [   88.486206] PPP Deflate Compression module registered
    [   88.491363] PPP BSD Compression module registered
    [   88.497222] PPP MPPE Compression module registered
    [   88.502075] NET: Registered protocol family 24
    [   88.506713] PPPoL2TP kernel driver, V1.0
    [   88.510681] dm9000 Ethernet Driver, V1.31
    [   88.515655] usbcore: registered new interface driver cdc_ether
    [   88.523223] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [   88.530273] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
    [   88.536651] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
    [   88.544311] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
    [   88.565521] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
    [   88.571502] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    [   88.578399] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [   88.585662] usb usb1: Product: OMAP-EHCI Host Controller
    [   88.591033] usb usb1: Manufacturer: Linux 2.6.32 ehci_hcd
    [   88.596496] usb usb1: SerialNumber: ehci-omap.0
    [   88.602233] hub 1-0:1.0: USB hub found
    [   88.606079] hub 1-0:1.0: 3 ports detected
    [   88.636383] usbcore: registered new interface driver cdc_acm
    [   88.642059] cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapters
    [   88.650695] Initializing USB Mass Storage driver...
    [   88.655944] usbcore: registered new interface driver usb-storage
    [   88.662048] USB Mass Storage support registered.
    [   88.667266] usbcore: registered new interface driver usbserial
    [   88.673126] usbserial: USB Serial Driver core
    [   88.678039] g_mass_storage gadget: Mass Storage Function, version: 2009/09/11
    [   88.685302] g_mass_storage gadget: Number of LUNs=1
    [   88.690216]  lun0: LUN: removable file: (no medium)
    [   88.695526] g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
    [   88.702575] g_mass_storage gadget: g_mass_storage ready
    [   88.707885] musb_hdrc musb_hdrc: MUSB HDRC host driver
    [   88.713684] musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 2
    [   88.721160] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
    [   88.728027] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [   88.735321] usb usb2: Product: MUSB HDRC host driver
    [   88.740356] usb usb2: Manufacturer: Linux 2.6.32 musb-hcd
    [   88.745819] usb usb2: SerialNumber: musb_hdrc
    [   88.751403] hub 2-0:1.0: USB hub found
    [   88.755249] hub 2-0:1.0: 1 port detected
    [   88.761016] mice: PS/2 mouse device common for all mice
    [   88.767425] ads7846 spi2.0: touchscreen, irq 187
    [   88.772430] ads7846 spi2.0: no device detected, test read result was 0x00000000
    [   88.781127] input: twl4030_pwrbutton as /devices/platform/i2c_omap.1/i2c-1/1-0049/twl4030_pwrbutton/input/input0
    [   88.793975] using rtc device, twl_rtc, for alarms
    [   88.798583] twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0
    [   88.805145] twl_rtc twl_rtc: Power up reset detected.
    [   88.810821] twl_rtc twl_rtc: Enabling TWL-RTC.
    [   88.816162] i2c /dev entries driver
    [   88.820892] Linux video capture interface: v2.00
    [   88.826477] usbcore: registered new interface driver uvcvideo
    [   88.832336] USB Video Class driver (v0.1.0)
    [   88.836547] Driver for 1-wire Dallas network protocol.
    [   88.842407] 1-Wire driver for the DS2760 battery monitor  chip  - (c) 2004-2005, Szabolcs Gyurko
    [   88.852172] OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
    [   88.932739] usb 1-2: new high speed USB device using ehci-omap and address 2
    [   88.964294] mmci-omap-hs mmci-omap-hs.1: err -16 configuring card detect
    [   88.972473] Registered led device: beagleboard::usr0
    [   88.977752] Registered led device: beagleboard::usr1
    [   88.983459] Registered led device: beagleboard::pmu_stat
    [   88.990570] usbcore: registered new interface driver usbhid
    [   88.996246] usbhid: USB HID core driver
    [   89.001159] logger: created 64K log 'log_main'
    [   89.006103] logger: created 256K log 'log_events'
    [   89.011230] logger: created 64K log 'log_radio'
    [   89.016113] logger: created 64K log 'log_system'
    [   89.021331] Advanced Linux Sound Architecture Driver Version 1.0.21.
    [   89.030120]
    [   89.030151] twl4030_modinit 2271
    [   89.092376] usb 1-2: New USB device found, idVendor=0424, idProduct=2514
    [   89.101013] usb 1-2: New USB device strings: Mfr=0, Product=0, SerialNumber=0
    [   89.109802] No device for DAI omap-mcbsp-dai-0
    [   89.114318] No device for DAI omap-mcbsp-dai-1
    [   89.118804] No device for DAI omap-mcbsp-dai-2
    [   89.123291] No device for DAI omap-mcbsp-dai-3
    [   89.127777] No device for DAI omap-mcbsp-dai-4
    [   89.132293] OMAP3 Beagle SoC init
    [   89.139343] hub 1-2:1.0: USB hub found
    [   89.143280]
    [   89.143280] twl4030_soc_probe2121
    [   89.148895] asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok
    [   89.154479]
    [   89.154479] twl4030_add_widgets1499
    [   89.160278]
    [   89.160278] twl4030_soc_probe2155
    [   89.166259] hub 1-2:1.0: 4 ports detected
    [   89.177673] ALSA device list:
    [   89.180664]   #0: omap3beagle (twl4030)
    [   89.185119] oprofile: using arm/armv7
    [   89.189056] TCP cubic registered
    [   89.192352] NET: Registered protocol family 17
    [   89.196868] NET: Registered protocol family 15
    [   89.201446] lib80211: common routines for IEEE802.11 drivers
    [   89.207183] ThumbEE CPU extension supported.
    [   89.211517] Power Management for TI OMAP3.

    This is what the output after booting from nand flash.

    Earlier it was stopping after uncompressing only, now what i have show above there it is stopping?

    AM3703 custom board using!

    Regards,

    santosh vastrad