J721S2XSOMXEVM: RTOS: PDK: ENET: Phy Linkup takes 4seconds, and only works in Auto-Negotiation mode

Part Number: J721S2XSOMXEVM

Tool/software:

Hi,

I am currently working with the CPSW2G, with GESI from mcu2_0. I see that the Phy Link Up always takes about 4000ms from the start of mcu2_0.

I had a look at the logs and found it is setting the mode to Full Duplex and 1GBit, so I tried to change the Mac LinkConfig(V3/enet_board_j721s2_evm.c) and Phy LinkConfig (EnetPhy_open); after that I don't see linkup at all.

Could you kindly let me know, how can I solve this issue?

In the end, I'd expect the Phy Link Up to happen much earlier than 4seconds.

Setup:

  • PDK 11.0
  • RTOS SDK 11.0
  • GESI Card - Static Eth Config in the lwip_example
  • Running on mcu2_0 started by uboot

Thank you.

Best,
Moses