Other Parts Discussed in Thread: AM1808
Hello,
i am trying to boot from NOR flash in AM1808 EVM, i have followed the next steps:
I have programmed ubl and u-boot in NOR Flash and it looks to boot Ok, u-boot version is 2010.12 and i have build it using Arago Toolchain in last SDK 5.03
Booting TI User Boot Loader
UBL Version: 1.65
UBL Flashtype: NOR
Starting NOR Copy...
CFI Query...passed.
NOR Initialization:
Command Set: Intel
Manufacturer: INTEL
Size: 0x00000008 MB
Valid magicnum, 0x55424CBB, found..
DONE
�FLASH: 8 MiBtry point at 0xC1080000.
MMC: davinci: 0
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
ARM Clock : 456000000 Hz
DDR Clock : 150000000 Hz
SF: Detected M25P64 with page size 256, total 8 MiB
Net: Ethernet PHY: GENERIC @ 0x00
DaVinci-EMAC
Hit any key to stop autoboot: 0
U-Boot >
Now i protect off and erase NOR to load uImage
U-Boot > protect off 0x60080000 +232b84
.................. done
Un-Protected 18 sectors
U-Boot > erase 0x60080000 +232b84
.................. done
Erased 18 sectors
Next i load the kernel in NOR after loading uImage in 0c0700000
Using DaVinci-EMAC device
TFTP from server 10.0.0.1; our IP address is 10.0.0.10
Filename 'uImage'.
Load address: 0xc0700000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#############################################################
done
Bytes transferred = 2304900 (232b84 hex)
U-Boot > cp.b c0700000 60080000 232b84
Copy to Flash... Flash not Erased
Is it Ok the message Copy to Flash...Flash not Erased?
Last i set bootcmd and boot
U-Boot > setenv bootcmd 'cp.b 60080000 c0700000 232b84;bootm'
U-Boot > boot
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2304836 Bytes = 2.2 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!
If from u-boot i download uImage from tftp directly to 0xc0700000 and boot, the booting is OK, so i guess that uImage is not being flashed Ok in NOR. Pls. could you help me?
Thanks in advance
Alberto