Part Number: LMG3100R017
Tool/software:
Hi,
We are currently evaluating the LMG3100R017 (GaN device with integrated gate driver) for use in a 3-phase BLDC motor inverter (reaction wheel application). We would like to confirm the following points:
-
Are there any adoption or reference cases of the LMG3100R017 in 3-phase BLDC motor applications?
-
Is there a possibility that a snubber circuit will be required? If so, would it be appropriate to place snubber pads between the DRN and SRC pins?
-
Since the driver and FET are integrated in a single package, what is the recommended method for evaluating the Safe Operating Area (SOA) during switching in practical measurements?
●Operating conditions
-
Application: 3-phase BLDC motor (reaction wheel) inverter circuit
-
Motor voltage range (Vds): 24V–34V
-
Switching frequency: 160kHz–240kHz
-
Current: 20A average, ΔI=10A ripple
We would appreciate your guidance on the above questions.
Best regards,
Conor