Other Parts Discussed in Thread: AM3517, AM3505
Hello,
Can you please help me with the questison below?
Thanks,
Todd
NAND Question: (In general, what is the largest size NAND flash the AM3517 can support?)
Can the AM3505/17 support any of the following NAND flash SLC memories:
4Gbit density, x16bit width
8Gbit density, x16bit width
16Gbit density, x16bit width
Our current design uses a 1Gbit, x16bit width SLC NAND device. We want to expand this memory size if possible.
DRAM Question: (In general, what is the largest size DDR2 memory the AM3517 can support?)
Can the AM3505/17 support 2 X DDR2 memories each with a 2Gbit (128Mbit x 16 bit width) density?
Our existing design uses 2 X 1Gbit (64Mbit x 16bit width) DDR2 memories for a total DDR2 memory of 256Mbytes. We want to expand this memory size if possible.
Display Subsystem Follow-up Question: (In general, we need LCD display support to get things up and running quickly, can your team help?)
We want to insure that the AM3517 can directly drive a large format LCD display without the need of converting from 24-bit parallel data to HDMI or DVI and then back to parallel data at the display. The AM3517 processor and its circuit card will be positioned behind the LCD display in this design allowing us to directly connect to the display and therefore minimize or eliminate cost associated with converting the display signals to HDMI or DVI. Is there someone on your team that can help with setting up the display registers in the AM3517 or at least confirm that a certain LCD display (to be picked soon) can be interfaced properly to the AM3517’s display sub-system? We don’t want to get so far down a design path and find out that it can’t be done.