Other Parts Discussed in Thread: TDA4VM
Tool/software:
Hi, TI experts,
I tried to add the trace configuration of the linux kernel in Veco's 9.2SDK as follows
BRs
regard
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi, TI experts,
I tried to add the trace configuration of the linux kernel in Veco's 9.2SDK as follows
BRs
regard
Hi,
Please see the following attached config which I have used with TDA4VM to get ftrace. Can you please compare and see if there are aany further config differences you need.
Regards,
Tanmay
Hi,
Can you confirm that without the ftrace changes, the system was working without any errors?
Is it possible to disable drm for timebeing and see what is happening?
What do you wish to do with the ftrace by the way?
Regards,
Tanmay
1. I confirm that the system is normal when I do not add trace
2. There is not only DRM in the error report, but also other modules, and it is useless to disable DRM alone. And it actually affects the activation of the R core
3. We have encountered some problems in resources and need this to assist in analysis
In addition, I did this on Veco's 9.2SDK
Hi,
Can you just share your entire config file used. I will try with this config on my end and see if I get the same issues.
Regards,
Tanmay
/cfs-file/__key/communityserver-discussions-components-files/791/2474.defconfig.txt
Please refer to this.